Building for imx6q and as I run ltib, hal's configure runs and echos:
Processing: hal
=================
Build path taken because: directory build, build key set, no prebuilt rpm,
rpmbuild --dbpath /home/mark/freescale/src/ltib/rootfs//var/lib/rpm --target arm --define '_unpackaged_files_terminate_build 0' --define '_target_cpu arm' --define '__strip strip' --define '_topdir /home/mark/freescale/src/ltib/rpm' --define '_prefix /usr' --define '_tmppath /home/mark/freescale/src/ltib/tmp' --define '_rpmdir /home/mark/freescale/src/ltib/rpm/RPMS' --define '_mandir /usr/share/man' --define '_sysconfdir /etc' --define '_localstatedir /var' -bc --short-circuit /home/mark/freescale/src/ltib/dist/lfs-5.1/hal/hal.spec
Building target platforms: arm
Building for target arm
Executing(%build): /bin/sh -e /home/mark/freescale/src/ltib/tmp/rpm-tmp.67640
+ umask 022
+ cd /home/mark/freescale/src/ltib/rpm/BUILD
+ cd hal-0.5.10
+ ./configure --prefix=/usr --host=arm-linux --build=x86_64-unknown-linux-gnu --enable-verbose-mode --with-hal-user=haldaemon --with-hal-group=haldaemon --with-backend=linux --with-dbus-sys=/usr/etc/dbus-1/system.d/ --with-cpufreq=no --with-usb-csr=no --with-pci-ids=/usr/share/ --with-usb-ids=/usr/share/
checking for a BSD-compatible install... /usr/bin/install -c
checking whether build environment is sane... yes
checking for a thread-safe mkdir -p... /bin/mkdir -p
checking for gawk... gawk
checking whether make sets $(MAKE)... yes
checking for arm-linux-strip... arm-linux-strip
checking whether to enable maintainer-specific portions of Makefiles... no
checking for style of include used by make... GNU
checking for arm-linux-gcc... gcc
checking for C compiler default output file name... a.out
checking whether the C compiler works... yes
checking whether we are cross compiling... yes
checking for suffix of executables...
checking for suffix of object files... o
checking whether we are using the GNU C compiler... yes
checking whether gcc accepts -g... yes
checking for gcc option to accept ISO C89... none needed
checking dependency style of gcc... gcc3
checking for library containing strerror... none required
checking for arm-linux-gcc... (cached) gcc
checking whether we are using the GNU C compiler... (cached) yes
checking whether gcc accepts -g... (cached) yes
checking for gcc option to accept ISO C89... (cached) none needed
checking dependency style of gcc... (cached) gcc3
checking whether gcc and cc understand -c and -o together... yes
checking how to run the C preprocessor... gcc -E
checking for grep that handles long lines and -e... /bin/grep
checking for egrep... /bin/grep -E
checking for ANSI C header files... yes
checking build system type... x86_64-unknown-linux-gnu
checking host system type... arm-unknown-linux-gnu
checking for a sed that does not truncate output... /bin/sed
checking for ld used by gcc... ld
checking if the linker (ld) is GNU ld... yes
checking for ld option to reload object files... -r
checking for BSD-compatible nm... /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-linux-nm -B
checking whether ln -s works... yes
checking how to recognize dependent libraries... pass_all
checking for sys/types.h... yes
checking for sys/stat.h... yes
checking for stdlib.h... yes
checking for string.h... yes
checking for memory.h... yes
checking for strings.h... yes
checking for inttypes.h... yes
checking for stdint.h... yes
checking for unistd.h... yes
checking dlfcn.h usability... yes
checking dlfcn.h presence... yes
checking for dlfcn.h... yes
checking whether we are using the GNU C++ compiler... yes
checking whether g++ accepts -g... yes
checking dependency style of g++... gcc3
checking how to run the C++ preprocessor... g++ -E
checking for arm-linux-g77... no
checking for arm-linux-xlf... no
checking for arm-linux-f77... no
checking for arm-linux-frt... no
checking for arm-linux-pgf77... no
checking for arm-linux-cf77... no
checking for arm-linux-fort77... no
checking for arm-linux-fl32... no
checking for arm-linux-af77... no
checking for arm-linux-xlf90... no
checking for arm-linux-f90... no
checking for arm-linux-pgf90... no
checking for arm-linux-pghpf... no
checking for arm-linux-epcf90... no
checking for arm-linux-gfortran... no
checking for arm-linux-g95... no
checking for arm-linux-xlf95... no
checking for arm-linux-f95... no
checking for arm-linux-fort... no
checking for arm-linux-ifort... no
checking for arm-linux-ifc... no
checking for arm-linux-efc... no
checking for arm-linux-pgf95... no
checking for arm-linux-lf95... no
checking for arm-linux-ftn... no
checking for g77... no
checking for xlf... no
checking for f77... no
checking for frt... no
checking for pgf77... no
checking for cf77... no
checking for fort77... no
checking for fl32... no
checking for af77... no
checking for xlf90... no
checking for f90... no
checking for pgf90... no
checking for pghpf... no
checking for epcf90... no
checking for gfortran... no
checking for g95... no
checking for xlf95... no
checking for f95... no
checking for fort... no
checking for ifort... no
checking for ifc... no
checking for efc... no
checking for pgf95... no
checking for lf95... no
checking for ftn... no
checking whether we are using the GNU Fortran 77 compiler... no
checking whether accepts -g... no
checking the maximum length of command line arguments... 1572864
checking command to parse /opt/freescale/usr/local/gcc-4.6.2-glibc-2.13-linaro-multilib-2011.12/fsl-linaro-toolchain/bin/arm-linux-nm -B output from gcc object... ok
checking for objdir... .libs
checking for arm-linux-ar... ar
checking for arm-linux-ranlib... arm-linux-ranlib
checking for arm-linux-strip... (cached) arm-linux-strip
checking if gcc supports -fno-rtti -fno-exceptions... no
checking for gcc option to produce PIC... -fPIC
checking if gcc PIC flag -fPIC works... yes
checking if gcc static flag -static works... yes
checking if gcc supports -c -o file.o... yes
checking whether the gcc linker (ld) supports shared libraries... yes
checking whether -lc should be explicitly linked in... no
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
checking whether stripping libraries is possible... yes
checking if libtool supports shared libraries... yes
checking whether to build shared libraries... yes
checking whether to build static libraries... yes
configure: creating libtool
appending configuration tag "CXX" to libtool
checking for ld used by g++... ld
checking if the linker (ld) is GNU ld... yes
checking whether the g++ linker (ld) supports shared libraries... yes
checking for g++ option to produce PIC... -fPIC
checking if g++ PIC flag -fPIC works... yes
checking if g++ static flag -static works... yes
checking if g++ supports -c -o file.o... yes
checking whether the g++ linker (ld) supports shared libraries... yes
checking dynamic linker characteristics... GNU/Linux ld.so
checking how to hardcode library paths into programs... immediate
appending configuration tag "F77" to libtool
checking whether make sets $(MAKE)... (cached) yes
checking whether ln -s works... yes
checking for special C compiler options needed for large files... no
checking for _FILE_OFFSET_BITS value needed for large files... 64
checking for arm-linux-pkg-config... no
checking for pkg-config... /opt/freescale/ltib/usr/bin/pkg-config
configure: WARNING: In the future, Autoconf will not detect cross-tools
whose name does not start with the host triplet. If you think this
configuration is useful to you, please write to autoconf@gnu.org.
checking pkg-config is at least version 0.9.0... yes
checking sys/ioccom.h usability... no
checking sys/ioccom.h presence... no
checking for sys/ioccom.h... no
checking sys/inotify.h usability... yes
checking sys/inotify.h presence... yes
checking for sys/inotify.h... yes
checking expat.h usability... yes
checking expat.h presence... yes
checking for expat.h... yes
checking for XML_ParserCreate in -lexpat... yes
checking usb.h usability... yes
checking usb.h presence... yes
checking for usb.h... yes
checking for usb_find_devices in -lusb... yes
checking for SMBIOSFreeMemory in -lsmbios... no
checking pci/pci.h usability... no
checking pci/pci.h presence... no
checking for pci/pci.h... no
checking for gperf... no
checking whether to rebuild gperf header files... checking for DBUS... yes
checking for GLIB... yes
checking for VOLUME_ID... yes
checking for pgoff_t... no
checking for BLKGETSIZE64... yes
checking for getgrouplist... yes
checking for asprintf... yes
checking for mallopt... yes
checking for strndup... yes
checking for xmlto... no
checking whether to build DocBook documentation... checking for xmllint... /usr/bin/xmllint
yes
checking for Sony PIC headers... yes
configure: creating ./config.status
config.status: creating hal.pc
config.status: creating hal-storage.pc
config.status: creating hal.conf
config.status: creating Makefile
config.status: creating hald/Makefile
config.status: creating hald/dummy/Makefile
config.status: creating hald/linux/Makefile
config.status: creating hald/linux/probing/Makefile
config.status: creating hald/linux/addons/Makefile
config.status: creating hald/solaris/Makefile
config.status: creating hald/solaris/probing/Makefile
config.status: creating hald/solaris/addons/Makefile
config.status: creating hald/freebsd/Makefile
config.status: creating hald/freebsd/probing/Makefile
config.status: creating hald/freebsd/libprobe/Makefile
config.status: creating hald/freebsd/addons/Makefile
config.status: creating hald-runner/Makefile
config.status: creating libhal/Makefile
config.status: creating libhal-storage/Makefile
config.status: creating tools/Makefile
config.status: creating tools/freebsd/Makefile
config.status: creating tools/linux/Makefile
config.status: creating partutil/Makefile
config.status: creating policy/Makefile
config.status: creating fdi/Makefile
config.status: creating fdi/information/Makefile
config.status: creating fdi/information/10freedesktop/Makefile
config.status: creating fdi/information/20thirdparty/Makefile
config.status: creating fdi/policy/Makefile
config.status: creating fdi/policy/10osvendor/Makefile
config.status: creating fdi/policy/20thirdparty/Makefile
config.status: creating fdi/preprobe/Makefile
config.status: creating fdi/preprobe/10freedesktop/Makefile
config.status: creating fdi/preprobe/20thirdparty/Makefile
config.status: creating doc/Makefile
config.status: creating doc/api/Makefile
config.status: creating doc/api/libhal/Makefile
config.status: creating doc/api/libhal/version.xml
config.status: creating doc/api/libhal-storage/Makefile
config.status: creating doc/api/libhal-storage/version.xml
config.status: creating doc/spec/Makefile
config.status: creating doc/spec/hal-spec.xml.in
config.status: creating doc/man/Makefile
config.status: creating config.h
config.status: config.h is unchanged
config.status: executing depfiles commands
HAL 0.5.10
==============
prefix: /usr
libdir: ${exec_prefix}/lib
libexecdir: ${exec_prefix}/libexec
bindir: ${exec_prefix}/bin
sbindir: ${exec_prefix}/sbin
datadir: ${datarootdir}
sysconfdir: ${prefix}/etc
localstatedir: ${prefix}/var
docdir: ${datarootdir}/doc/${PACKAGE_TARNAME}
dbus-1 system.d dir: /usr/etc/dbus-1/system.d/
pci.ids dir: /usr/share/
usb.ids dir: /usr/share/
compiler: gcc
cflags: -g -O2 -Wall -Wchar-subscripts -Wmissing-declarations -Wnested-externs -Wpointer-arith -Wcast-align -Wsign-compare
ldflags: -Wl,--as-needed
cppflags:
xmlto: no
xmllint: /usr/bin/xmllint
User for HAL: haldaemon
Group for HAL: haldaemon
hald pidfile: ${prefix}/var/run/hald/pid
hald socket dir: ${prefix}/var/run/hald
eject program: /usr/bin/eject
OS backend: linux
use acpi kernel interface: yes
use acpid interface: yes
use libusb: yes
use libpci: no
use libparted: no
use gperf: no
use PolicyKit: no
use ConsoleKit: no
use ACL management: no
use umount.hal helper: no
use ACPI: yes
use PMU: yes
use APM: yes
use Sony PIC: yes
Macbook backlight support: no (Linux only, x86 only, requires libpci)
Macbook Pro utils: no (Linux only, x86 only, requires libpci)
OMAP utils: yes (Linux only, arm only)
CPU frequency scaling: no (Linux only)
Re-map multimedia keys: no (Linux only, requires gperf)
Forward IBM ACPI events: no (Linux only)
Forward Toshiba ACPI events: no (Linux only)
USB wireless mouse power: no (Linux only, requires libusb)
Dell Backlight: no (Linux only, requires libsmbios >= 0.13.4)
Maintainer mode: no
Building verbose mode: yes
Building api docs: no
Building docs: no
Building man pages: yes
NOTE: building with verbose mode increases library size, may slightly
increase security risk, and decreases performance.
NOTE: You have to install init scripts yourself and tweak your own policy
NOTE: Remember to create user haldaemon and group haldaemon before make install
NOTE: For development, use run-hald.sh and debug-hald.sh scripts in hald/ to
use programs (callouts, probers, addons) and device information files
from build directories. You may still need 'make install' to
install the udev rule to receive events from udev.
and then make runs, and does its stuff. But dies with several lines like:
gcc -g -O2 -Wall -Wchar-subscripts -Wmissing-declarations -Wnested-externs -Wpointer-arith -Wcast-align -Wsign-compare -Wl,--as-needed -o .libs/hald-probe-input probe-input.o logger.o ../../../libhal/.libs/libhal.so -L/home/mark/freescale/src/ltib/rootfs/usr/lib -ldbus-1 -lusb /usr/lib/libusb.so
/usr/lib/libusb.so: file not recognized: File format not recognized
collect2: ld returned 1 exit status
make[5]: *** [hald-probe-serial] Error 1
I'm sure due to parallel make, there's several of these all complaining about /usr/lib/libusb.so.
I've dug into hal's configure and Makefile (and little into hal.spec), but for the life of me, I can't see how it picks up /usr/lib/libusb.so. The valid (arm) one can be found from the -L and -l switches. Any idea on either how to get the extra libusb.so out of the gcc command, or at least why it ends up there?
Hi Peter,
have you tried the clean previous compilation and building again? move to the source code folder and type make clean, then build again. This has worked for me for the type of errors you are getting.
Leo
Finally, to workaround on this error I backup my original /usr/lib/libusb.so at my Ubuntu host machine, copy the target 's libusb.so from rootfs/usr/lib/libusb-0.1.4.4.0 to /usr/lib/libusb.so. Luckily it works! (Please restore the original /usr/lib/libusb.so after build!)
It looks the "hal-0.5.10" is referring to the wrong path for the target's libusb.so, perhaps something goes wrong with the configure or build scripts. I don't have the knowledge to fix the error. Does anyone know how to fix this?
Hi Pete,
Modify the Makefile, then create a patched recipe (spec) with the command
./ltib -p <package name> -m patchmerge
Now remove the rpm/BUILD/<package name>
and execute the ltib's triad prep-scbuild-scdeploy. That ltib way to patch autobuild tools and source code.
Leo
sorry, I typo, -L should link to a lib directory, not a file.
so please try to add the LDFLAGS in the configure like this. ./configure LDFLAGS="-L/home/lucid/ltib/rootfs/usr/lib" .......
So you can modify the hal.spec file in ltib.
ltib will set the gcc compiler to correct version. If you don't use ltib to build, you need set the gcc to correct path.
you can try "ltib -m shell". In the shell, you can run "gcc -v", then you can see the gcc version like
gcc version 4.6.2 20110630 (prerelease) (Freescale MAD -- Linaro 2011.07 -- Built at 2011/08/10 09:20)
You can try to build the package in the shell with the script.
-Grace
That helps. But, my build environment has been subject to repeated changes, so I probably won't get a chance to really nail this down for a bit. Current SWAG is autoconf/configure or how they're called....