Hi,
we successfully connected an 800x480 lvds display to the sabreboard. The console and the yocoto splashscreen looks fine, but the XServer will not start.
I think there are some problems with the changed resolution. Using the XGA Display everything works fine.
Perhaps anybody has an idea what this could be.
The Xorg.log looks like this:
[244440.009] _XSERVTransSocketOpenCOTSServer: Unable to open socket for inet6
[244440.009] _XSERVTransOpen: transport open failed for inet6/imx6qsabresd:0
[244440.009] _XSERVTransMakeAllCOTSServerListeners: failed to open listener for inet6
[244440.016]
X.Org X Server 1.11.2
Release Date: 2011-11-04
[244440.016] X Protocol Version 11, Revision 0
[244440.016] Build Operating System: Linux 3.5.0-23-generic x86_64
[244440.016] Current Operating System: Linux imx6qsabresd 3.0.35-12.09.01+yocto+g0596856 #19 SMP PREEMPT Tue Apr 16 17:33:29 CEST 2013 armv7l
[244440.017] Kernel command line: console=ttymxc0,115200 root=/dev/mmcblk1p2 rootwait rw video=mxcfb0:dev=ldb,LDB-LG,if=RGB24
[244440.017] Build Date: 11 April 2013 12:55:00PM
[244440.017]
[244440.017] Current version of pixman: 0.27.2
[244440.017] Before reporting problems, check http://wiki.x.org
to make sure that you have the latest version.
[244440.017] Markers: (--) probed, (**) from config file, (==) default setting,
(++) from command line, (!!) notice, (II) informational,
(WW) warning, (EE) error, (NI) not implemented, (??) unknown.
[244440.017] (==) Log file: "/var/log/Xorg.0.log", Time: Mon Apr 15 16:40:40 2013
[244440.020] (==) Using config file: "/etc/X11/xorg.conf"
[244440.020] (==) Using system config directory "/usr/share/X11/xorg.conf.d"
[244440.022] (==) No Layout section. Using the first Screen section.
[244440.022] (==) No screen section available. Using defaults.
[244440.022] (**) |-->Screen "Default Screen Section" (0)
[244440.022] (**) | |-->Monitor "<default monitor>"
[244440.029] (==) No device specified for screen "Default Screen Section".
Using the first device section listed.
[244440.029] (**) | |-->Device "i.MX Accelerated Framebuffer Device"
[244440.029] (==) No monitor specified for screen "Default Screen Section".
Using a default monitor configuration.
[244440.029] (**) Option "BlankTime" "0"
[244440.029] (**) Option "StandbyTime" "0"
[244440.029] (**) Option "SuspendTime" "0"
[244440.029] (**) Option "OffTime" "0"
[244440.029] (==) Automatically adding devices
[244440.029] (==) Automatically enabling devices
[244440.030] (WW) The directory "/usr/share/fonts/X11/misc/" does not exist.
[244440.030] Entry deleted from font path.
[244440.030] (WW) The directory "/usr/share/fonts/X11/TTF/" does not exist.
[244440.031] Entry deleted from font path.
[244440.031] (WW) The directory "/usr/share/fonts/X11/OTF/" does not exist.
[244440.031] Entry deleted from font path.
[244440.031] (WW) The directory "/usr/share/fonts/X11/Type1/" does not exist.
[244440.031] Entry deleted from font path.
[244440.031] (WW) The directory "/usr/share/fonts/X11/100dpi/" does not exist.
[244440.031] Entry deleted from font path.
[244440.031] (WW) The directory "/usr/share/fonts/X11/75dpi/" does not exist.
[244440.031] Entry deleted from font path.
[244440.031] (==) FontPath set to:
[244440.031] (==) ModulePath set to "/usr/lib/xorg/modules"
[244440.031] (II) The server relies on udev to provide the list of input devices.
If no devices become available, reconfigure udev or disable AutoAddDevices.
[244440.031] (II) Loader magic: 0x17e940
[244440.031] (II) Module ABI versions:
[244440.031] X.Org ANSI C Emulation: 0.4
[244440.031] X.Org Video Driver: 11.0
[244440.031] X.Org XInput driver : 13.0
[244440.031] X.Org Server Extension : 6.0
[244440.031] (II) Open APM successful
[244440.031] (II) LoadModule: "extmod"
[244440.047] (WW) Warning, couldn't open module extmod
[244440.047] (II) UnloadModule: "extmod"
[244440.047] (II) Unloading extmod
[244440.047] (EE) Failed to load module "extmod" (module does not exist, 0)
[244440.047] (II) LoadModule: "dbe"
[244440.047] (WW) Warning, couldn't open module dbe
[244440.047] (II) UnloadModule: "dbe"
[244440.047] (II) Unloading dbe
[244440.047] (EE) Failed to load module "dbe" (module does not exist, 0)
[244440.047] (II) LoadModule: "glx"
[244440.047] (WW) Warning, couldn't open module glx
[244440.048] (II) UnloadModule: "glx"
[244440.048] (II) Unloading glx
[244440.048] (EE) Failed to load module "glx" (module does not exist, 0)
[244440.048] (II) LoadModule: "dri"
[244440.048] (WW) Warning, couldn't open module dri
[244440.048] (II) UnloadModule: "dri"
[244440.048] (II) Unloading dri
[244440.048] (EE) Failed to load module "dri" (module does not exist, 0)
[244440.048] (II) LoadModule: "dri2"
[244440.048] (WW) Warning, couldn't open module dri2
[244440.048] (II) UnloadModule: "dri2"
[244440.048] (II) Unloading dri2
[244440.048] (EE) Failed to load module "dri2" (module does not exist, 0)
[244440.048] (II) LoadModule: "vivante"
[244440.048] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so
[244440.105] (II) Module vivante: vendor="X.Org Foundation"
[244440.105] compiled for 1.11.2, module version = 1.0.0
[244440.105] ABI class: X.Org Video Driver, version 11.0
[244440.105] (II) VIVANTE: fb driver for vivante: VivanteGC500, VivanteGC2100,
VivanteGCCORE
[244440.105] (--) using VT number 1
[244440.170] (WW) Falling back to old probe method for vivante
[244440.170] (II) Loading sub module "fbdevhw"
[244440.170] (II) LoadModule: "fbdevhw"
[244440.170] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so
[244440.172] (II) Module fbdevhw: vendor="X.Org Foundation"
[244440.172] compiled for 1.11.2, module version = 0.0.2
[244440.172] ABI class: X.Org Video Driver, version 11.0
[244440.172] (II) Loading /usr/lib/xorg/modules/drivers/vivante_drv.so
[244440.172] (II) Loading /usr/lib/xorg/modules/libfbdevhw.so
[244440.173] (II) VIVANTE(0): using default device
[244440.173] (WW) VGA arbiter: cannot open kernel arbiter, no multi-card support
[244440.173] (II) VIVANTE(0): Creating default Display subsection in Screen section
"Default Screen Section" for depth/fbbpp 16/16
[244440.173] (==) VIVANTE(0): Depth 16, (==) framebuffer bpp 16
[244440.173] (==) VIVANTE(0): RGB weight 565
[244440.173] (==) VIVANTE(0): Default visual is TrueColor
[244440.173] (==) VIVANTE(0): Using gamma correction (1.0, 1.0, 1.0)
[244440.173] (II) VIVANTE(0): hardware: DISP4 BG (video memory: 750kB)
[244440.173] (II) VIVANTE(0): checking modes against framebuffer device...
[244440.173] (II) VIVANTE(0): checking modes against monitor...
[244440.173] (--) VIVANTE(0): Virtual size is 800x480 (pitch 800)
[244440.174] (**) VIVANTE(0): Built-in mode "current": 33.3 MHz, 31.8 kHz, 60.6 Hz
[244440.174] (II) VIVANTE(0): Modeline "current"x0.0 33.26 800 840 845 1045 480 490 495 525 -hsync -vsync -csync (31.8 kHz)
[244440.174] (==) VIVANTE(0): DPI set to (96, 96)
[244440.174] (II) Loading sub module "fb"
[244440.174] (II) LoadModule: "fb"
[244440.174] (II) Loading /usr/lib/xorg/modules/libfb.so
[244440.207] (II) Module fb: vendor="X.Org Foundation"
[244440.208] compiled for 1.11.2, module version = 1.0.0
[244440.208] ABI class: X.Org ANSI C Emulation, version 0.4
[244440.208] (II) Loading sub module "exa"
[244440.208] (II) LoadModule: "exa"
[244440.208] (II) Loading /usr/lib/xorg/modules/libexa.so
[244440.215] (II) Module exa: vendor="X.Org Foundation"
[244440.215] compiled for 1.11.2, module version = 2.5.0
[244440.215] ABI class: X.Org Video Driver, version 11.0
[244440.271] (II) VIVANTE(0): FB Start = 0x32d4c000 FB Base = 0x32d4c000 FB Offset = (nil)
[244440.282] (II) VIVANTE(0): test Initializing EXA
[244440.282] (II) EXA(0): Driver allocated offscreen pixmaps
[244440.282] (II) EXA(0): Driver registered support for the following operations:
[244440.282] (II) Solid
[244440.283] (II) Copy
[244440.283] (II) Composite (RENDER acceleration)
[244440.283] (II) UploadToScreen
[244440.296] (==) VIVANTE(0): Backing store disabled
[244440.297] (==) VIVANTE(0): DPMS enabled
[244440.297] (==) RandR enabled
[244440.297] (II) Initializing built-in extension Generic Event Extension
[244440.297] (II) Initializing built-in extension SHAPE
[244440.297] (II) Initializing built-in extension MIT-SHM
[244440.298] (II) Initializing built-in extension XInputExtension
[244440.298] (II) Initializing built-in extension XTEST
[244440.298] (II) Initializing built-in extension BIG-REQUESTS
[244440.298] (II) Initializing built-in extension SYNC
[244440.298] (II) Initializing built-in extension XKEYBOARD
[244440.298] (II) Initializing built-in extension XC-MISC
[244440.298] (II) Initializing built-in extension XFIXES
[244440.298] (II) Initializing built-in extension RENDER
[244440.298] (II) Initializing built-in extension RANDR
[244440.298] (II) Initializing built-in extension COMPOSITE
[244440.298] (II) Initializing built-in extension DAMAGE
[244440.564] (II) config/udev: Adding input device LITEON Technology USB Multimedia Keyboard (/dev/input/event5)
[244440.564] (**) LITEON Technology USB Multimedia Keyboard: Applying InputClass "evdev keyboard catchall"
[244440.564] (II) LoadModule: "evdev"
[244440.564] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[244440.568] (II) Module evdev: vendor="X.Org Foundation"
[244440.568] compiled for 1.11.2, module version = 2.7.0
[244440.568] Module class: X.Org XInput Driver
[244440.568] ABI class: X.Org XInput driver, version 13.0
[244440.568] (II) Using input driver 'evdev' for 'LITEON Technology USB Multimedia Keyboard'
[244440.568] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[244440.568] (**) LITEON Technology USB Multimedia Keyboard: always reports core events
[244440.568] (**) evdev: LITEON Technology USB Multimedia Keyboard: Device: "/dev/input/event5"
[244440.568] (--) evdev: LITEON Technology USB Multimedia Keyboard: Vendor 0x46d Product 0xc312
[244440.568] (--) evdev: LITEON Technology USB Multimedia Keyboard: Found keys
[244440.568] (II) evdev: LITEON Technology USB Multimedia Keyboard: Configuring as keyboard
[244440.568] (**) Option "config_info" "udev:/sys/devices/platform/fsl-ehci.0/usb1/1-1/1-1:1.0/input/input5/event5"
[244440.568] (II) XINPUT: Adding extended input device "LITEON Technology USB Multimedia Keyboard" (type: KEYBOARD, id 6)
[244440.568] (**) Option "xkb_rules" "evdev"
[244440.568] (**) Option "xkb_model" "evdev"
[244440.568] (**) Option "xkb_layout" "us"
[244440.645] (II) config/udev: Adding input device gpio-keys (/dev/input/event0)
[244440.645] (**) gpio-keys: Applying InputClass "evdev keyboard catchall"
[244440.645] (II) Using input driver 'evdev' for 'gpio-keys'
[244440.645] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[244440.646] (**) gpio-keys: always reports core events
[244440.646] (**) evdev: gpio-keys: Device: "/dev/input/event0"
[244440.646] (--) evdev: gpio-keys: Vendor 0x1 Product 0x1
[244440.646] (--) evdev: gpio-keys: Found keys
[244440.646] (II) evdev: gpio-keys: Configuring as keyboard
[244440.646] (**) Option "config_info" "udev:/sys/devices/platform/gpio-keys/input/input0/event0"
[244440.646] (II) XINPUT: Adding extended input device "gpio-keys" (type: KEYBOARD, id 7)
[244440.646] (**) Option "xkb_rules" "evdev"
[244440.646] (**) Option "xkb_model" "evdev"
[244440.646] (**) Option "xkb_layout" "us"
[244440.648] (II) config/udev: Adding input device WM8962 Beep Generator (/dev/input/event6)
[244440.648] (II) No input driver/identifier specified (ignoring)
[244440.649] (II) config/udev: Adding input device max11801_ts (/dev/input/event1)
[244440.649] (**) max11801_ts: Applying InputClass "evdev touchscreen catchall"
[244440.649] (II) Using input driver 'evdev' for 'max11801_ts'
[244440.649] (II) Loading /usr/lib/xorg/modules/input/evdev_drv.so
[244440.649] (**) max11801_ts: always reports core events
[244440.649] (**) evdev: max11801_ts: Device: "/dev/input/event1"
[244440.649] (--) evdev: max11801_ts: Vendor 0 Product 0
[244440.649] (--) evdev: max11801_ts: Found absolute axes
[244440.649] (--) evdev: max11801_ts: Found x and y absolute axes
[244440.649] (--) evdev: max11801_ts: Found absolute touchscreen
[244440.649] (II) evdev: max11801_ts: Configuring as touchscreen
[244440.650] (**) evdev: max11801_ts: YAxisMapping: buttons 4 and 5
[244440.650] (**) evdev: max11801_ts: EmulateWheelButton: 4, EmulateWheelInertia: 10, EmulateWheelTimeout: 200
[244440.650] (**) Option "config_info" "udev:/sys/devices/platform/imx-i2c.1/i2c-1/1-0048/input/input1/event1"
[244440.650] (II) XINPUT: Adding extended input device "max11801_ts" (type: TOUCHSCREEN, id 8)
[244440.650] (II) evdev: max11801_ts: initialized for absolute axes.
[244440.650] (**) max11801_ts: (accel) keeping acceleration scheme 1
[244440.650] (**) max11801_ts: (accel) acceleration profile 0
[244440.650] (**) max11801_ts: (accel) acceleration factor: 2.000
[244440.651] (**) max11801_ts: (accel) acceleration threshold: 4
[244440.651] (II) config/udev: Adding input device max11801_ts (/dev/input/mouse0)
[244440.651] (II) No input driver/identifier specified (ignoring)
[244440.653] (II) config/udev: Adding input device isl29023 light sensor (/dev/input/event2)
[244440.653] (II) No input driver/identifier specified (ignoring)
[244440.654] (II) config/udev: Adding input device mag3110 (/dev/input/event3)
[244440.654] (II) No input driver/identifier specified (ignoring)
[244440.655] (II) config/udev: Adding input device mma845x (/dev/input/event4)
[244440.655] (II) No input driver/identifier specified (ignoring)
[244441.337] (II) evdev: LITEON Technology USB Multimedia Keyboard: Close
[244441.337] (II) UnloadModule: "evdev"
[244441.337] (II) Unloading evdev
[244441.607] (II) evdev: gpio-keys: Close
[244441.607] (II) UnloadModule: "evdev"
[244441.607] (II) Unloading evdev
[244441.927] (II) evdev: max11801_ts: Close
[244441.927] (II) UnloadModule: "evdev"
[244441.927] (II) Unloading evdev
[244441.928] (II) VIVANTE(0): Shutdown EXA
[244442.036] Server terminated successfully (0). Closing log file.
已解决! 转到解答。