Hi,
I try to display over hdmi a video encoded in H.264 with a bitrate of 499kbps and an audio stereo track encoded in MPEG-4 AAC with a bitrate of 93 kbps with gstreamer 1.0 on my iMX6Q.
When I use a pipeline without audio, I have no problem :
gst-launch-1.0 filesrc location=/media/mmcblk1p1/FILE0_5MinSyncTest.mp4 ! video/quicktime ! aiurdemux ! vpudec ! imxv4l2sink
But when I add audio in the pipeline :
gst-launch-1.0 filesrc location=/media/mmcblk1p1/FILE0_5MinSyncTest.mp4 ! video/quicktime ! aiurdemux name=demux demux. ! queue ! vpudec ! imxv4l2sink demux. ! queue ! beepdec ! alsasink
I have timestamping proble :
There may be a timestamping problem, or this computer is too slow.
If I add sync="false" to imxv4l2sink element there is no more timestamping problem but the sound is offset from the video.
I can play video with bigger bitrate without audio, I have no timestamping problem.
Is there a solution to fix this timestamping problem ?
已解决! 转到解答。
I set "max-size-time=0" to queues and it solve the problem.
It miss some frame but the result is quite good.
This command failed with the following log :
gst-launch-1.0 playbin uri=file:///media/mmcblk1p1/FILE0_5MinSyncTest.mp4
Setting pipeline to PAUSED ...
Pipeline is PREROLLING ...
====== AIUR: 4.0.8 build on May 25 2016 08:46:26. ======
Core: MPEG4PARSER_06.09.17 build on Aug 13 2015 10:41:12
file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm11_elinux.so.3.2
------------------------
Track 00 [video_0] Enabled
Duration: 0:05:00.267008000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)avc, width=(int)640, height=(int)480, framerate=(fraction)30000/1001, codec_data=(buffer)014d401effe10
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:05:00.350016000
Language: und
Mime:
audio/mpeg, mpegversion=(int)4, channels=(int)2, rate=(int)44100, bitrate=(int)93588, stream-format=(string)raw, codec_data=(buffer)1208
------------------------
display(/dev/fb0) resolution is (1920x1080).
====== OVERLAYSINK: 4.0.8 build on May 25 2016 08:46:41. ======
display(/dev/fb0) resolution is (1920x1080).
[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
====== BEEP: 4.0.8 build on May 25 2016 08:46:30. ======
Core: AAC decoder Wrapper build on Apr 22 2014 09:43:50
file: /usr/lib/imx-mm/audio-codec/wrap/lib_aacd_wrap_arm12_elinux.so.3
CODEC: BLN_MAD-MMCODECS_AACD_ARM_03.09.00_CORTEX-A8 build on Jun 19 2014 18:30:32.
display(/dev/fb0) resolution [ 467.220340] mxc_v4l2_output v4l2_out.34: Bypass IC.
is (1920x1080).
[ 467.229116] mxc_v4l2_output v4l2_out.34: Bypass IC.
gst-launch-1.0: ../imxvpuapi/imxvpuapi_vpulib.c:2349: imx_vpu_dec_mark_framebuffer_as_displayed: Assertion `framebuffer != ((void *)0)' failed.
Aborted