Problem while booting from uSD card on i.MX6UL custom board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem while booting from uSD card on i.MX6UL custom board

2,495 次查看
punitkumar
Contributor IV

Hi

I have connected my custom i.MX6UL board to uSD card and try to download image using mfgtool but failing and following messages appear on console

U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+gd7d7c43 (Aug 29 2016 - 12:46:14)
CPU:   Freescale i.MX6UL rev1.0 at 396 MHz
CPU:   Temperature 34 C
Reset cause: POR
Board: MX6UL 14X14 LPDDR2 ARM2
I2C:   ready
DRAM:  256 MiB
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
MMC init failed
Using default environment
unsupported panel TFT43AB
In:    serial
Out:   serial
Err:   serial
Card did not respond to voltage select!
Net:   Ethernet@0x20b4000 is fused, disable it
FEC1 MXC: board_eth_init:failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x80800000 [ 0x000000 - 0x552da8 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7550025 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300b895
Modify /soc/aips-bus@02000000/tsc@02040000:status disabled
Modify /soc/aips-bus@02100000/sim@0218c000:status disabled
Modify /soc/aips-bus@02100000/sim@021b4000:status disabled
Modify /soc/aips-bus@02000000/can@02090000:status disabled
Modify /soc/aips-bus@02000000/can@02094000:status disabled
Modify /soc/aips-bus@02100000/lcdif@021c8000:status disabled
Modify /soc/aips-bus@02100000/pxp@021cc000:status disabled
Modify /soc/aips-bus@02100000/csi@021c4000:status disabled
Modify /soc/aips-bus@02000000/ethernet@020b4000:status disabled
Modify /soc/aips-bus@02100000/caam@2140000:status disabled
Modify /soc/aips-bus@02100000/usb@02184200:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@0202c000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@02030000:status disabled
Modify /soc/aips-bus@02000000/bee@02044000:status disabled
Modify /soc/aips-bus@02100000/serial@021f4000:status disabled
Modify /soc/aips-bus@02100000/serial@021fc000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02018000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02024000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f0000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f4000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f8000:status disabled
Modify /soc/aips-bus@02000000/pwm@020fc000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02010000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02014000:status disabled
Modify /soc/aips-bus@02100000/i2c@021a8000:status disabled
Modify /soc/aips-bus@02100000/i2c@021f8000:status disabled
Modify /soc/aips-bus@02000000/gpt@020e8000:status disabled
Modify /soc/aips-bus@02000000/epit@020d4000:status disabled
ft_system_setup for mx6
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 4.1.15-1.1.1-mfgtool+gd5d7c02 (pratyush@pratyushGeotech) (gcc version 5.2.0 (GCC) ) #1 SMP PREEMPT Thu Aug 25 18:09:22 IST 2016
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
Reserved memory: failed to allocate memory for node 'linux,cma'
cma: Failed to reserve 320 MiB
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8fdd3000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 241860K/262144K available (6895K kernel code, 319K rwdata, 2396K rodata, 388K init, 423K bss, 20284K reserved, 0K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0x90800000 - 0xff000000   (1768 MB)
    lowmem  : 0x80000000 - 0x90000000   ( 256 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x8091af88   (9292 kB)
      .init : 0x8091b000 - 0x8097c000   ( 388 kB)
      .data : 0x8097c000 - 0x809cbf00   ( 320 kB)
       .bss : 0x809ce000 - 0x80a37f14   ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082f0
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7376K (83800000 - 83f34000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 218, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 7e:74:e1:13:79:b7
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
VSD_3V3: disabling
can-3v3: disabling
clk: Not disabling unused clocks
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 388K (8091b000 - 8097c000)
Starting UTP
uuc 0.5 [built Aug 25 2016 18:16:02]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk0'
UTP: executing "sh mksdcard.sh /dev/mmcblk0"
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
also when I tried booting the board by downloading the image externally, the board shows no response but the same image runs in EVK successfully.
can someone help me over the issue.
I'm using uSD card on SDHC1 port on i.MX6UL.
Regards
Punit Kumar
标签 (3)
0 项奖励
回复
3 回复数

1,229 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Punit

from log "Board: MX6UL 14X14 LPDDR2 ARM2", seems this is lpdddr2

board, while EVK uses ddr3 memory. So if you are using lpddr2, image

should be rebuilt for that memory and first ddr test should be run

https://community.freescale.com/docs/DOC-105652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,229 次查看
punitkumar
Contributor IV

Thanks igorpadykov

But this image was working with our other i.MX6UL custom board having same hardware configuration and the only difference was the previous board is having eMMC on uSDHC2 port and this board is having uSD card on uSDHC1 port.

Please have a look at below log-

U-Boot 2015.04-imx_v2015.04_4.1.15_1.0.0_ga+gd7d7c43 (Mar 02 2017 - 19:02:08)
CPU:   Freescale i.MX6UL rev1.0 at 396 MHz
CPU:   Temperature 35 C
Reset cause: POR
Board: MX6UL 14X14 LPDDR2 ARM2
I2C:   ready
DRAM:  256 MiB
MMC:   FSL_SDHC: 0
*** Warning - bad CRC, using default environment
unsupported panel TFT43AB
In:    serial
Out:   serial
Err:   serial
switch to partitions #0, OK
mmc0 is current device
Net:   Ethernet@0x20b4000 is fused, disable it
FEC1 MXC: board_eth_init:failed
No ethernet found.
Boot from USB for mfgtools
Use default environment for                              mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot:  0
Kernel image @ 0x80800000 [ 0x000000 - 0x553c20 ]
## Loading init Ramdisk from Legacy Image at 83800000 ...
   Image Name:   fsl-image-mfgtool-initramfs-imx6
   Image Type:   ARM Linux RAMDisk Image (gzip compressed)
   Data Size:    7550208 Bytes = 7.2 MiB
   Load Address: 00000000
   Entry Point:  00000000
   Verifying Checksum ... OK
## Flattened Device Tree blob at 83000000
   Booting using the fdt blob at 0x83000000
   Using Device Tree in place at 83000000, end 8300b895
Modify /soc/aips-bus@02000000/tsc@02040000:status disabled
Modify /soc/aips-bus@02100000/sim@0218c000:status disabled
Modify /soc/aips-bus@02100000/sim@021b4000:status disabled
Modify /soc/aips-bus@02000000/can@02090000:status disabled
Modify /soc/aips-bus@02000000/can@02094000:status disabled
Modify /soc/aips-bus@02100000/lcdif@021c8000:status disabled
Modify /soc/aips-bus@02100000/pxp@021cc000:status disabled
Modify /soc/aips-bus@02100000/csi@021c4000:status disabled
Modify /soc/aips-bus@02000000/ethernet@020b4000:status disabled
Modify /soc/aips-bus@02100000/caam@2140000:status disabled
Modify /soc/aips-bus@02100000/usb@02184200:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@0202c000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/sai@02030000:status disabled
Modify /soc/aips-bus@02000000/bee@02044000:status disabled
Modify /soc/aips-bus@02100000/serial@021f4000:status disabled
Modify /soc/aips-bus@02100000/serial@021fc000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02018000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/serial@02024000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f0000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f4000:status disabled
Modify /soc/aips-bus@02000000/pwm@020f8000:status disabled
Modify /soc/aips-bus@02000000/pwm@020fc000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02010000:status disabled
Modify /soc/aips-bus@02000000/spba-bus@02000000/ecspi@02014000:status disabled
Modify /soc/aips-bus@02100000/i2c@021a8000:status disabled
Modify /soc/aips-bus@02100000/i2c@021f8000:status disabled
Modify /soc/aips-bus@02000000/gpt@020e8000:status disabled
Modify /soc/aips-bus@02000000/epit@020d4000:status disabled
ft_system_setup for mx6
Starting kernel ...
Booting Linux on physical CPU 0x0
Linux version 4.1.15-1.1.1-mfgtool+gd5d7c02 (pratyush@pratyush) (gcc version 5.2.0 (GCC) ) #2 SMP PREEMPT Wed Mar 1 10:59:54 IST 2017
CPU: ARMv7 Processor [410fc075] revision 5 (ARMv7), cr=10c5387d
CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
Machine model: Freescale i.MX6 UltraLite 14x14 EVK Board
Reserved memory: failed to allocate memory for node 'linux,cma'
cma: Failed to reserve 320 MiB
Memory policy: Data cache writealloc
PERCPU: Embedded 12 pages/cpu @8fdd3000 s16768 r8192 d24192 u49152
Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 65024
Kernel command line: console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.file=/fat g_mass_storage.ro=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber= clk_ignore_unused
PID hash table entries: 1024 (order: 0, 4096 bytes)
Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
Memory: 241848K/262144K available (6899K kernel code, 321K rwdata, 2400K rodata, 388K init, 423K bss, 20296K reserved, 0K cma-reserved, 0K highmem)
Virtual kernel memory layout:
    vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    vmalloc : 0x90800000 - 0xff000000   (1768 MB)
    lowmem  : 0x80000000 - 0x90000000   ( 256 MB)
    pkmap   : 0x7fe00000 - 0x80000000   (   2 MB)
    modules : 0x7f000000 - 0x7fe00000   (  14 MB)
      .text : 0x80008000 - 0x8091cfa0   (9300 kB)
      .init : 0x8091d000 - 0x8097e000   ( 388 kB)
      .data : 0x8097e000 - 0x809ce5c0   ( 322 kB)
       .bss : 0x809d1000 - 0x80a3af54   ( 424 kB)
SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Preemptible hierarchical RCU implementation.
        Additional per-CPU info printed with stalls.
        RCU restricting CPUs from NR_CPUS=4 to nr_cpu_ids=1.
RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1
NR_IRQS:16 nr_irqs:16 16
mxc_clocksource_init 24000000
Switching to timer-based delay loop, resolution 41ns
sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
Console: colour dummy device 80x30
Calibrating delay loop (skipped), value calculated using timer frequency.. 48.00 BogoMIPS (lpj=240000)
pid_max: default: 32768 minimum: 301
Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
/cpus/cpu@0 missing clock-frequency property
CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
Setting up static identity map for 0x80008280 - 0x800082f0
Brought up 1 CPUs
SMP: Total of 1 processors activated (48.00 BogoMIPS).
CPU: All CPU(s) started in SVC mode.
devtmpfs: initialized
device-tree: Duplicate name in lcdif@021c8000, renamed to "display#1"
VFP support v0.3: implementor 41 architecture 2 part 30 variant 7 rev 5
clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
pinctrl core: initialized pinctrl subsystem
NET: Registered protocol family 16
DMA: preallocated 256 KiB pool for atomic coherent allocations
cpuidle: using governor ladder
cpuidle: using governor menu
hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
hw-breakpoint: maximum watchpoint size is 8 bytes.
imx6ul-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
mxs-dma 1804000.dma-apbh: initialized
SCSI subsystem initialized
usbcore: registered new interface driver usbfs
usbcore: registered new interface driver hub
usbcore: registered new device driver usb
i2c i2c-0: IMX I2C adapter registered
i2c i2c-0: can't use DMA
i2c i2c-1: IMX I2C adapter registered
i2c i2c-1: can't use DMA
Linux video capture interface: v2.00
pps_core: LinuxPPS API ver. 1 registered
pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
PTP clock support registered
Advanced Linux Sound Architecture Driver Initialized.
Switched to clocksource mxc_timer1
NET: Registered protocol family 2
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 2048 (order: 2, 16384 bytes)
TCP: Hash tables configured (established 2048 bind 2048)
UDP hash table entries: 256 (order: 1, 8192 bytes)
UDP-Lite hash table entries: 256 (order: 1, 8192 bytes)
NET: Registered protocol family 1
RPC: Registered named UNIX socket transport module.
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
Freeing initrd memory: 7376K (83800000 - 83f34000)
imx rpmsg driver is registered.
Bus freq driver module loaded
futex hash table entries: 256 (order: 2, 16384 bytes)
VFS: Disk quotas dquot_6.6.0
VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
NFS: Registering the id_resolver key type
Key type id_resolver registered
Key type id_legacy registered
jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
fuse init (API version 7.23)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
imx-weim 21b8000.weim: Driver registered.
backlight supply power not found, using dummy regulator
imx-sdma 20ec000.sdma: no event needs to be remapped
imx-sdma 20ec000.sdma: loaded firmware 3.3
imx-sdma 20ec000.sdma: initialized
2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 19, base_baud = 5000000) is a IMX
console [ttymxc0] enabled
21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 218, base_baud = 5000000) is a IMX
imx sema4 driver is registered.
[drm] Initialized drm 1.1.0 20060810
[drm] Initialized vivante 1.0.0 20120216 on minor 0
brd: module loaded
loop: module loaded
fsl-quadspi 21e0000.qspi: unrecognized JEDEC id bytes: ff, ff, ff
fsl-quadspi 21e0000.qspi: Freescale QuadSPI probe failed
2188000.ethernet supply phy not found, using dummy regulator
pps pps0: new PPS source ptp0
fec 2188000.ethernet (unnamed net_device) (uninitialized): Invalid MAC address: 00:00:00:00:00:00
fec 2188000.ethernet (unnamed net_device) (uninitialized): Using random MAC address: 06:74:d9:e9:f7:67
libphy: fec_enet_mii_bus: probed
fec 2188000.ethernet eth0: registered PHC device 0
ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
ehci-mxc: Freescale On-Chip EHCI Host driver
usbcore: registered new interface driver usb-storage
2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
2184000.usb supply vbus not found, using dummy regulator
Mass Storage Function, version: 2009/09/11
LUN: removable file: (no medium)
LUN: removable read only file: /fat
Number of LUNs=1
Number of LUNs=1
g_mass_storage gadget: Mass Storage Gadget, version: 2009/09/11
g_mass_storage gadget: g_mass_storage ready
mousedev: PS/2 mouse device common for all mice
input: 20cc000.snvs:snvs-powerkey as /devices/platform/soc/2000000.aips-bus/20cc000.snvs/20cc000.snvs:snvs-powerkey/input/input0
snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
i2c /dev entries driver
IR NEC protocol handler initialized
IR RC5(x/sz) protocol handler initialized
IR RC6 protocol handler initialized
IR JVC protocol handler initialized
IR Sony protocol handler initialized
IR SANYO protocol handler initialized
IR Sharp protocol handler initialized
IR MCE Keyboard/mouse protocol handler initialized
IR XMP protocol handler initialized
pxp-v4l2 pxp_v4l2: initialized
imx2-wdt 20bc000.wdog: use WDOG_B to reboot.
imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
sdhci: Secure Digital Host Controller Interface driver
sdhci: Copyright(c) Pierre Ossman
sdhci-pltfm: SDHCI platform and OF driver helper
/soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
/soc/aips-bus@02100000/usdhc@02194000: voltage-ranges unspecified
sdhci-esdhc-imx 2194000.usdhc: No vmmc regulator found
sdhci-esdhc-imx 2194000.usdhc: No vqmmc regulator found
g_mass_storage gadget: high-speed config #1: Linux File-Backed Storage
mmc1: SDHCI controller on 2194000.usdhc [2194000.usdhc] using ADMA
usbcore: registered new interface driver usbhid
usbhid: USB HID core driver
NET: Registered protocol family 10
sit: IPv6 over IPv4 tunneling driver
NET: Registered protocol family 17
Key type dns_resolver registered
Registering SWP/SWPB emulation handler
snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01 00:00:00 UTC (0)
VSD_3V3: disabling
can-3v3: disabling
clk: Not disabling unused clocks
ALSA device list:
  No soundcards found.
Freeing unused kernel memory: 388K (8091d000 - 8097e000)
Starting UTP
uuc 0.5 [built Mar  1 2017 10:44:28]
UTP: Waiting for device to appear
UTP: file/device node /dev/utp already exists
cpu_id is 0
UTP: received command 'send'
UTP: sending Success to kernel for command send.
UTP: received command '$ tar xf $FILE '
UTP: executing "tar xf $FILE "
UTP: sending Success to kernel for command $ tar xf $FILE .
utp_poll: pass returned.
UTP: received command '$ sh mksdcard.sh /dev/mmcblk0'
UTP: executing "sh mksdcard.sh /dev/mmcblk0"
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
“wait for /dev/mmcblk0 appear”
earlier, there was some hardware connection bug and due to this we were getting "MMC init failed" in previous log.
But it's resolved now. But we are still not able to get any further.
DDR calibration is already done and the following values were updated in cfg file and new u-boot.imx was generated.
Read calibration
   MPRDDLCTL PHY0 (0x021b0848) = 0x40404A50
   Write calibration
   MPWRDLCTL PHY0 (0x021b0850) = 0x40405048
Is there anything else we need to do for DDR calibration?
Regards
Punit Kumar
0 项奖励
回复

1,229 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Punit

please run ddr test and rebuild uboot with new calibration settings (update uboot/.../board_name/*.cfg)

obtained from test

https://community.freescale.com/docs/DOC-105652 

Best regards
igor

0 项奖励
回复