Hi,
I'm working on a custom board based on an iMX6 solo X (ref.: MCIMX6X1CVO08AB).
On the SD3 port, i have a WL1805 module which works in 1V8. The SD3 port is powered by NVCC_HIGH(3V1 on my board) and NVCC_LOW (1V8).
I am booting from an eMMC on SD4 port from fuse. In Table 5-6. MMC/eMMC Boot Fusemap,BOOT_CFG2[1] is use for setting SD3 voltage. Is BOOT_CFG2[1] worked only when booting from SD3, or it could be use in my case for setting the SD3 port power when booting from SD4 ?
If not, how can i set SD3 power to NVCC_LOW in linux ?
Thanks for your help,
Hi ambroisealgrin
BOOT_CFG2[1] works also when booting from SD4,
in linux one can set LVE bit in IPOMUX pad register
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
Thanks for your answer. As you said, i set the fuse to 1, i had a level of 2.2V on my IOs, which lokk like a conflict between the external 1V8 Pull up and the iMx voltage.
So i set LVE bit and i still have this conflict.
Did i make something wrong ?
Fuse read in uboot is : |
---|
Normal Boot Hit any key to stop autoboot: 0 => fuse read 0 5 Reading bank 0: Word 0x00000005: 00005a61 |
DTS configuration |
---|
&usdhc3 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_usdhc3>; bus-width = <4>; cap-power-off-card; keep-power-in-suspend; status = "okay"; wlcore: wlcore@2 { compatible = "ti,wl1805"; reg = <2>; }; }; pinctrl_usdhc3: usdhc3grp { fsl,pins = < MX6SX_PAD_SD3_CMD__USDHC3_CMD 0x417059 MX6SX_PAD_SD3_CLK__USDHC3_CLK 0x410059 MX6SX_PAD_SD3_DATA0__USDHC3_DATA0 0x417059 MX6SX_PAD_SD3_DATA1__USDHC3_DATA1 0x417059 MX6SX_PAD_SD3_DATA2__USDHC3_DATA2 0x417059 MX6SX_PAD_SD3_DATA3__USDHC3_DATA3 0x417059 MX6SX_PAD_SD3_DATA4__GPIO7_IO_6 0x41b0b0 MX6SX_PAD_SD3_DATA5__GPIO7_IO_7 0x41b0b0 >; }; |
Hi igorpadykov,
Sorry for the long time to answer, i checked the register and the LVE bit was unset.
I tried a new approach by setting the port in 1V8 in uboot.
The LVE option wasn't avalaible for imx6sx, in a first time i just had "(1 << 22)" in the iomux_v3_cfg_t. Didn't work.
So i did some change iomux-v3.c/.h and now adding PAD_CTL_LVE in the struct iomux_v3_cfg_t make SD3 pads working in 1V8 in uboot (see attached file).
I think it should be a similar problem for the linux part.