Power dissipation and Junction temperature of MCIMX286CVM4B

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power dissipation and Junction temperature of MCIMX286CVM4B

820件の閲覧回数
rakshith_manjun
Contributor II

Hi, I am working on calculating the power dissipation of MCIMX286CVM4B based on the current consumption on each of the power rail (See below) . All of the power source is from the internal DC/DC buck regulator of IMX286 without any battery connected. With the help of a software to measure the junction temperature, the software reads out 60°C at 24°C ambient. Doing the math with 36°C/W of thermal resistance considering 6-layer PCB, the total power dissipated is 1.0 Watt. The 5V power source to internal buck regulators measures 0.204 Amps giving 1.02 Watt of input power, this is what confuses me. How can power dissipation be almost equal to consumption. Am I doing anything incorrect? 

VDDIO(3.3V) = 0.0215 Amps ---> 0.0709 Watt 

VDDA (1.8V) = 0.0903 Amps ---> 0.1625 Watt

VDDD (1.2V) = 0.252 Amps ---> 0.3027 Watt                                            

Total -----------------------------------> 0.53625 Watt ( consumption ) 

Since I have the above consumption data, the 5V source measures 1.02 Watt including dissipation of lower voltage power rails. Therefore the dissipation should be 1.02 - 0.53625 = 0.4837 Watt of power dissipation resulting in 42.4°C of junction temperature, which is not the case. 

The processor is exposed to air at 24°C ambient and on a 6-layer PCB. 

Please advise. your inputs on this is much appreciated.

Thank you.

Best regards,

Rakshith Manjunath

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

752件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rakshith

right, power dissipation is almost equal to consumption since

most current from these supplies is consumed by i.MX28 internally.

For example VDDD current is consumed by i.MX28 core.

Power supplies usage is described in AN4199

Using the i.MX28 Power Management Unit and Battery Charger

Typical i.MX28 VDDIO,VDDA,VDDD consumption can be found in Table 12

i.MX28 Applications Processors for Consumer Products

Also one can take into account temperature sensor accuracy https://community.nxp.com/thread/468500 

and dcdc efficiency (about 85%).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛