Power-Up Behaviour Reset Pin

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power-Up Behaviour Reset Pin

328件の閲覧回数
alaskora_byk_mstang
Contributor I
Hi 
We are using imx8mp based custom  board.
The resetout pin of our SOMs with Smarc 2.1 interface is defined as P126. It is expected that this pin should be low at the initial moment and later transition to high.
However, in our system,the board is powered the reset pin remains low.
What might be the reason for this, and how can we fix it?
Screenshot from 2023-12-04 13-49-28.png

ラベル(1)
0 件の賞賛
返信
1 返信

312件の閲覧回数
JorgeCas
NXP TechSupport
NXP TechSupport

Hello, I hope you are doing well.

Maybe this could be caused by the power-up sequence present on your SOM board, so I suggest check the PMIC. I do not have access to the documentation of your product.

Best regards.

0 件の賞賛
返信