Power Consumption ratings in i.MX8M Datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Power Consumption ratings in i.MX8M Datasheet

跳至解决方案
1,101 次查看
arnemaathuis
Contributor II

Hello,


In paragraph 3.1.5 of the i.MX8M Nano Datasheet (IMX8NCEC) maximum supply currents of the device are mentioned.

However, no information is given on which device(Single, Dual or Quad Core, Lite) these currents are measured.

Can i assume that the ratings for e.g.the VDD_ARM rail of the QuadLite differ from the ratings of the DualLite?

Is there any information available on power consumption for each individual variant? Im very interested in the ratings for the i.MX 8M Nano DualLite(MIMX8MN3DVTJZAA), for which i am currently designing a board for.

Regard Arne Maathuis, Sintecs, NL

标签 (2)
0 项奖励
回复
1 解答
913 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Arne Maathuis,

The maximum supply currents shown are for reference and would refer to the Quad variant of the processor. Ratings for a variant of the i.MX8M Nano Dual Lite should be lower than those of the Quad Lite, just as you assume.

We don’t have a maximum supply current for each variant. In this situation I would recommend using Application Note 12410 as reference where some power consumptions estimates are shown for some real-life scenarios. (Please keep in mind these are for the i.MX8M, but they may serve as a counterpoint to the maximum supply currents on the i.MX8M Nano datasheet, I would recommend that you at least fulfill the power for the scenarios on the AN)

https://www.nxp.com/docs/en/application-note/AN12410.pdf

My apologies for the inconvenience.
Regards,

在原帖中查看解决方案

0 项奖励
回复
1 回复
914 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Arne Maathuis,

The maximum supply currents shown are for reference and would refer to the Quad variant of the processor. Ratings for a variant of the i.MX8M Nano Dual Lite should be lower than those of the Quad Lite, just as you assume.

We don’t have a maximum supply current for each variant. In this situation I would recommend using Application Note 12410 as reference where some power consumptions estimates are shown for some real-life scenarios. (Please keep in mind these are for the i.MX8M, but they may serve as a counterpoint to the maximum supply currents on the i.MX8M Nano datasheet, I would recommend that you at least fulfill the power for the scenarios on the AN)

https://www.nxp.com/docs/en/application-note/AN12410.pdf

My apologies for the inconvenience.
Regards,

0 项奖励
回复