Porting AGL(Automotive Grade Linux) onto I.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting AGL(Automotive Grade Linux) onto I.MX6

3,715件の閲覧回数
saimadhusudhank
Contributor I

Hi ,

I want to port AGL on to our I.MX6 based board .Can any one suggest where to start and where to get the base Kernel package for it?

Reference for AGL

https://www.automotivelinux.org/

Thanks,

Saimadhusudhan

ラベル(2)
2 返答(返信)

1,642件の閲覧回数
CarlChien
NXP Employee
NXP Employee

Hi Saimadhusudhan

Here are some informaito for your reference.

Regarding AGL, one demo is under NXP git sever. See http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/.

For details, you can refer to README http://git.freescale.com/git/cgit.cgi/imx/meta-nxp-agl.git/tree/README.txt?h=krogoth

 

Please note it’s demo, provided “as is”.

 

Best regards,

Carl

0 件の賞賛

1,642件の閲覧回数
art
NXP Employee
NXP Employee

Various basic packages of i.MX6 Linux BSPs for various Linux kernel versions and i.MX6 processor types can be found here:

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛