Pop and offsets at start of audio playback/record on imx28evk on 3.14 kernel

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pop and offsets at start of audio playback/record on imx28evk on 3.14 kernel

744 Views
CraigMcQueen
Contributor III

I'm testing the 3.14.19 kernel on imx28evk, with a Yocto build that uses the linux-fslc kernel provider.

Playback

When doing SGTL5000 audio playback on the imx28evk on 3.14 kernel, I notice that the audio "fades in" over the first (approximately) 500 ms of playback. This is very noticeable and not ideal in certain applications (e.g. audio notifications that are of short duration).

However, if audio playback starts while audio recording is already in-progress, then there is no fade-in; instead there is a loud pop. I assume the fade-in is there to mask the pop. The pop is very unpleasant through headphones.

I didn't think either the pop or the fade-in occurred on the 2.6.35 kernel. How feasible is it to improve the driver to avoid or reduce the pop, and remove the necessity for a fade-in? Or, make the fade-in faster so it doesn't so noticeably change the audio output?

Record

When recording, I notice there is a low-frequency ramping offset at the start of a recording (after the 400-500 ms of previous audio) of approx 600-700 ms duration. This also reduces the audio quality at the start of the recording. It could potentially cause clipping of a loud signal, or otherwise reduce the quality of captured audio depending on the application usage. It could cause a pop on playback (local playback or e.g. VoIP transmission to a remote device). It could reduce the audio quality through an audio CODEC.

How feasible is it to improve the driver to avoid a ramping offset at the start of recording?

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

532 Views
fabio_estevam
NXP Employee
NXP Employee

Please try it on 3.18-rc4.

0 Kudos
Reply

532 Views
CraigMcQueen
Contributor III

I've built a 3.18-rc4 kernel. I retested these issues, and found that they are still present under that kernel, for both playback and record.

0 Kudos
Reply