I'm trying to use Qt to play back a video. Here is my code:
// Play a video.
QApplication app(argc, argv);
qDebug("Try to play a video: %s", argv[1]);
QVideoWidget* videoWidget = new QVideoWidget;
videoWidget->setFullScreen(true);
QMediaPlayer* player = new QMediaPlayer;
player->setVideoOutput(videoWidget);
player->setMedia(QUrl::fromLocalFile(argv[1]));
player->play();
videoWidget->show();
return app.exec();
Unfortunately when I execute this code on my iMX6Q board (which normally has no problems using gst-launch to play back video) I end up with a series of static vertical lines appearing on the monitor and no video.
What do I need to do to get video working from Qt?
Here is the output on the console by the way when I try to play back a video using the code above:
# /usr/local/smartfade2/Console /usr/sample720p60_40Mbps.mp4
mxc_sdc_fb fb.26: 1280x720 h_sync,r,l: 40,110,220 v_sync,l,u: 5,5,20 pixclock=74250000 Hz
Try to play a video: /usr/sample720p60_40Mbps.mp4
(gst-plugin-scanner:446): GStreamer-CRITICAL **: gst_element_class_add_pad_template: assertion 'GST_IS_PAD_TEMPLATE (templ)' failed
(gst-plugin-scanner:446): GStreamer-WARNING **: Failed to load plugin '/usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so': /usr/lib/imx-mm/audio-codec/lib_src_ppp_arm11_elinux.so: undefined symbol: src_up2_prefilter_proc
(Console:442): GStreamer-CRITICAL **: gst_object_ref_sink: assertion 'GST_IS_OBJECT (object)' failed
This plugin does not support setParent!
This plugin does not support setParent!
[INFO] Product Info: i.MX6Q/D/S
vpudec versions :smileyhappy:
plugin: 3.0.11
wrapper: 1.0.46(VPUWRAPPER_ARM_LINUX Build on Feb 16 2015 14:50:08)
vpulib: 5.4.23
firmware: 3.1.1.46056
[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0
Thanks,
Ralph
Is this solved?
I faced same problem with slight different output as follows:
QIconvCodec::convertToUnicode: using Latin-1 for conversion, iconv_open failed
QIconvCodec::convertFromUnicode: using Latin-1 for conversion, iconv_open failed
(<unknown>:3577): GStreamer-CRITICAL **: gst_object_ref_sink: assertion `GST_IS_OBJECT (object)' failed
This plugin does not support setParent!
This plugin does not support setParent!
This plugin does not support setParent!
This plugin does not support setParent!
Could not open file
Aiur: 3.0.7
Core: AVI_PARSER_03.05.07 build on Mar 27 2013 10:06:13
mime: video/x-msvideo
file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///root/640x360_mpeg4.mp4
Idx File:
/root/.aiur/.root.640x360_mpeg4.mp4.aidx
Seekable : Yes
Size(byte): 34551532
Movie Info:
Seekable : Yes
Live : No
Duration : 0:03:43.451428000
ReadMode : File
Track : 2
Track 00 [video_000000] Enabled
Duration: 0:03:43.280000000
Language: und
Mime:
video/x-xvid, width=(int)640, height=(int)360, framerate=(fraction)25/1
[INFO] Product Info: i.MX6Q/D/S
vpudec versions :smileyhappy:
plugin: 3.0.7
wrapper: 1.0.35(VPUWRAPPER_ARM_LINUX Build on May 20 2015 07:21:32)
vpulib: 5.4.16
firmware: 2.3.10.40778
Track 01 [audio_000000] Enabled
Duration: 0:03:43.451428000
Language: und
Mime:
audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)2, rate=(int
)44100, bitrate=(int)224000
[INFO] bitstreamMode 1, chromaInterleave 1, mapType 0, tiled2LinearEnable 0
Beep: 3.0.7
Core: MP3 decoder Wrapper build on Mar 15 2013 09:57:40
mime: audio/mpeg, mpegversion = (int)1
file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so
CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_CORTEX-A8 build on Dec 5 2012 09:45:19.
It's been a few weeks since I did this, however I think my code was like this:
qDebug("Try to play a video: %s", argv[1]);
QVideoWidget* videoWidget = new QVideoWidget;
videoWidget->setFullScreen(true);
QMediaPlayer* player = new QMediaPlayer;
player->setVideoOutput(videoWidget);
player->setMedia(QUrl::fromLocalFile(argv[1]));
player->play();
videoWidget->show();
Thanks,
Ralph