Play video with Nuplayer on android_L5.0.0_1.0.1 is stuttering

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Play video with Nuplayer on android_L5.0.0_1.0.1 is stuttering

1,059件の閲覧回数
felixhsu
Contributor III

Hi All

Our customer has updated their Android version from L5.0.0_1.0.0 to L5.0.0_1.0.1 by our official released patch.

 

The product they designed has dual display output.

 

So, they tested dual 1080p30 MPEG4/MPEG2 video at the same time.

 

But the video is stuttering when using Nuplayer under L5.0.0_1.0.1, but L5.0.0_1.0.0 isn't.

 

They also tried to use GMplayer to play the video,It doesn't have this kind of issue on these two version of android.

 

 

We read the log of Nuplayer to play this MPEG4 video under L5.0.0_1.0.1.

 

 

 

 

01-01 00:01:29.992 E/OMXNodeInstance(  158): OMX_SetParameter() failed for StoreMetaDataInBuffers: 0x8000101a

 

01-01 00:01:29.992 E/ACodec  (  158): [OMX.Freescale.std.video_decoder.mpeg4.hw-based] storeMetaDataInBuffers failed w/ err -2147483648

 

...

 

01-01 00:01:30.067 E/NuPlayer(  158): feedDecoderInputData getCurrentPosition failed.

 

01-01 00:01:30.073 E/NuPlayer(  158): feedDecoderInputData getCurrentPosition failed.

 

01-01 00:01:30.073 E/NuPlayer(  158): feedDecoderInputData getCurrentPosition failed.

 

...

 

01-01 00:01:30.406 E/ACodec  (  158): dequeueBuffer failed.

 

...

 

01-01 00:01:31.137 I/NuPlayerRenderer(  158): possible video time jump of 684ms, retrying in 10ms

 

01-01 00:01:31.147 I/NuPlayerRenderer(  158): possible video time jump of 674ms, retrying in 10ms

 

01-01 00:01:31.158 I/NuPlayerRenderer(  158): possible video time jump of 661ms, retrying in 500ms

 

----------------------------------------------------------------------------------------------------------------------------------------------------------------

 

Is it any related change of the L5.0.0_1.0.1 patch will cause this video stuttering issue?

 

or any additional configuration we need to apply?

ラベル(4)
0 件の賞賛
2 返答(返信)

521件の閲覧回数
mumintsao
Contributor I

This issue will happen on version L5.0.0_1.0.0 as well, and this issue can be reproduce in NXP's reference board.

0 件の賞賛

521件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

I got information that this is from  Google native code print out, no fix plan

0 件の賞賛