Hallo all :
my board in enet(pg1) is the same of mx6qsabresd-AI(pg2) ,so I use the same code in my uboot of enet ,but it is error:
pg1
pg2
U-Boot 2015.04-14468-gd7d7c43-dirty (Jun 20 2016 - 10:23:24)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 32 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: MMC/SD: Reset never completed.
voltage not supported by controller
SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 1 not found
PHY reset timed out
phy_test:test
FEC [PRIME]
Error: FEC address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=>
Thanks
Original Attachment has been moved to: mymx6q.c.zip
已解决! 转到解答。
Thank you very much for pointing me, According to your ideas successfully solved the problem, Thank you very much!!!
U-Boot 2015.04-14468-gd7d7c43-dirty (Jun 21 2016 - 19:23:09)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 47 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
MMC: FSL_SDHC: 0
SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB
In: serial
Out: serial
Err: serial
Net: FEC [PRIME]
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=>
Hi xuhui
on mx6qsabresd-AI PHYADDRESS0,1=10, while on your schematic both 0.
In general one can also check definitions in include/configs/boardfile.h :
"#define CONFIG_FEC_MXC_PHYADDR"
and add debug codes to ../drivers/net/fec_mxc.c
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igorpadykov
Thank you for your reply so quickly!with you tips,I edit the file mx6sabre_common.h
"#define CONFIG_FEC_MXC_PHYADDR 1" to #define CONFIG_FEC_MXC_PHYADDR 0"
but it is the same problem .
U-Boot 2015.04-14468-gd7d7c43-dirty (Jun 20 2016 - 18:14:59)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 51 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: MMC/SD: Reset never completed.
voltage not supported by controller
SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB
*** Warning - bad CRC, using default environment
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 0 not found
PHY reset timed out
phy_test:test
FEC [PRIME]
Error: FEC address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=> mii info
PHY 0x04: OUI = 0x1374, Model = 0x07, Rev = 0x04, 10baseT, HDX
=> mii dump 0 0
0. (ffff) -- PHY control register --
(8000:8000) 0.15 = 1 reset
(4000:4000) 0.14 = 1 loopback
(2040:2040) 0. 6,13 = b11 speed selection = 10 Mbps
(1000:1000) 0.12 = 1 A/N enable
(0800:0800) 0.11 = 1 power-downThanks
(0400:0400) 0.10 = 1 isolate
(0200:0200) 0. 9 = 1 restart A/N
(0100:0100) 0. 8 = 1 duplex = full
(0080:0080) 0. 7 = 1 collision test enable
(003f:003f) 0. 5- 0 = 63 (reserved)
=> mii dump 1 0
0. (ffff) -- PHY control register --
(8000:8000) 0.15 = 1 reset
(4000:4000) 0.14 = 1 loopback
(2040:2040) 0. 6,13 = b11 speed selection = 10 Mbps
(1000:1000) 0.12 = 1 A/N enable
(0800:0800) 0.11 = 1 power-down
(0400:0400) 0.10 = 1 isolate
(0200:0200) 0. 9 = 1 restart A/N
(0100:0100) 0. 8 = 1 duplex = full
(0080:0080) 0. 7 = 1 collision test enable
(003f:003f) 0. 5- 0 = 63 (reserved)
=>
I have no idea in this
Thanks
I change the
define CONFIG_FEC_MXC_PHYADDR 0x04,but
U-Boot 2015.04-14468-gd7d7c43-dirty (Jun 20 2016 - 20:14:08)
CPU: Freescale i.MX6Q rev1.5 at 792 MHz
CPU: Temperature 49 C
Reset cause: POR
Board: MX6Q-Sabreauto revA
I2C: ready
DRAM: 1 GiB
PMIC: PFUZE100 ID=0x10
NAND: 0 MiB
MMC: MMC/SD: Reset never completed.
voltage not supported by controller
SF: Detected M25P32 with page size 256 Bytes, erase size 64 KiB, total 4 MiB
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: serial
Err: serial
Net: Phy 4 not found
PHY reset timed out
phy_test:test
FEC [PRIME]
Error: FEC address not set.
Boot from USB for mfgtools
Use default environment for mfgtools
Run bootcmd_mfg: run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};
Hit any key to stop autoboot: 0
Bad Linux ARM zImage magic!
=> mii info
PHY 0x00: OUI = 0x1374, Model = 0x07, Rev = 0x04, 10baseT, HDX
=>