Performance of i.MX6SoloX GbE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Performance of i.MX6SoloX GbE

Jump to solution
798 Views
ko-hey
Senior Contributor II

Hi all

I want to know about network performance of i.MX6SoloX GbE.

According to RM, SoloX has two GbE channels.

Can these channels achieve 1000 Mbps transfer rate for each?

To be frank, I'm concerning about following community's answer.

https://community.freescale.com/message/391842#391842

Is that errata not applicable to SoloX ?

Please let me know.

Ko-hey

Labels (1)
Tags (2)
0 Kudos
1 Solution
591 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

SoloX can achieve 1000 Mbps transfer rate for each

(Errata: ERR004512 not applicable to it).

Below description of improvements

MX6SLX  Ethernet.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
592 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

SoloX can achieve 1000 Mbps transfer rate for each

(Errata: ERR004512 not applicable to it).

Below description of improvements

MX6SLX  Ethernet.jpg

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
591 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you.

Do you have measured value data ?

Ko-hey

0 Kudos