PORTING ANDROID TO i.MX23evk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PORTING ANDROID TO i.MX23evk

跳至解决方案
1,523 次查看
shanmugamsundar
Contributor IV

hi all,

        I am new to i.MX23 evk, i want to port the android on the evk, is it possible to port it?, can any one help me, if its so plz share me how to get the linux android BSP for i.MX23evk,

Thanks,

shan

标签 (4)
0 项奖励
1 解答
1,065 次查看
MT
NXP Employee
NXP Employee
0 项奖励
4 回复数
1,066 次查看
MT
NXP Employee
NXP Employee

I believe that Allgo Embedded a Freescale Partner did an Android port.

http://www.freescale.com/webapp/dap.detail.framework?CUSTOMER=ALEMR&company=ALLGO%2BEMBEDDED%2BSYSTE...

0 项奖励
1,066 次查看
hippo
NXP TechSupport
NXP TechSupport

Freescale has no Android port for the i.MX233 processor and no plans to make it. The main reason is that this processor seems to have not enough performance to provide convenient operation of Android OS on it. The main Android-targeted members of the i.MX processors family are now i.MX51, i.MX53, and i,MX6.

Please look at link below for supported BSPs (Linux, WinCE)

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX23_SW

1,065 次查看
shanmugamsundar
Contributor IV

hi hippo,

    i had downloaded the Linux kernel source for i.MX233, in that i need to port QT GUI application, can you help me on how to port the QT and cross compiling the source.

Thanks,

shan

0 项奖励
1,065 次查看
Yuri
NXP Employee
NXP Employee

The following may be helpful :

All Boards Qt v2

0 项奖励