Hii Team ,
I go through with the below link document :
https://www.nxp.com/docs/en/application-note/AN11697.pdf
But I am facing an issue with it , that pn5xx driver is compiled .ko and .o files are created but after implement the image in imx8mm board , there is no any message I am getting in the boot-up process .
Below are my changes in kernel :
############# dts file changes : ######################
/* ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ */
pinctrl_i2c4: i2c4grp {
fsl,pins = <
MX8MM_IOMUXC_I2C4_SCL_I2C4_SCL 0x400001c3
MX8MM_IOMUXC_I2C4_SDA_I2C4_SDA 0x400001c3
>;
};
---------------------
&i2c4{
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_i2c4>;
status = "okay";
pn547: pn547@28 { compatible = "nxp,pn547";
reg = <0x28>;
gpio-controller;
clock-frequency = <400000>;
interrupt-gpios = <&gpio3 24 0>;
enable-gpios = <&gpio4 11 0>;
};
};
pinctrl_sai1: sai1grp {
fsl,pins = <
MX8MM_IOMUXC_SAI1_MCLK_SAI1_MCLK 0xd6
MX8MM_IOMUXC_SAI1_TXFS_SAI1_TX_SYNC 0xd6
MX8MM_IOMUXC_SAI1_RXD7_SAI1_TX_SYNC 0xd6
MX8MM_IOMUXC_SAI1_TXC_GPIO4_IO11 0x19 /* Changes done for pn5xx */
------------------------------------
pinctrl_sai3: sai3grp {
fsl,pins = <
MX8MM_IOMUXC_SAI3_TXFS_SAI3_TX_SYNC 0xd6
MX8MM_IOMUXC_SAI3_TXC_SAI3_TX_BCLK 0xd6
MX8MM_IOMUXC_SAI3_MCLK_SAI3_MCLK 0xd6
MX8MM_IOMUXC_SAI3_TXD_SAI3_TX_DATA0 0xd6
/* MX8MM_IOMUXC_I2C4_SDA_GPIO5_IO21 0xd6 */
>;
===============================================================
BR
Pramod