PMIC for i.MX8DualXPlus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC for i.MX8DualXPlus

1,430 Views
bimal
Contributor III

HI,

For oneof our project we are planning to use the i.MX8DulxPlus Part# MIMX8DX5CVLFZAC (Without DSP) will be using LPDDR4.

For which i have query regarding the selection of PMIC part# As per the processor we need industrial grade PMIC part compatible for i.MX8DualxPlus and as per the datasheet of PMIC 33PF8100 there are several parts as below:

1) MC34PF8100FJEP Industrial grade compatible with LPDDR4 

2) MC33PF8100FJES Automotive grade compatible with LPDDR4

We should go with the part#1 in above list, is this correct as per latest OTP programming support on this PMIC?

Or we should go with the other latest OTP programming ID from FJ??

Require your input to quickly converge on this.

Tags (2)
3 Replies

1,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bimal

yes  MC34PF8100FJEP is correct selection for

industrial grade part with LPDDR4.


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,363 Views
bimal
Contributor III

HI Igor,

Thanks for the prompt response,

Can you also let me know the difference between below parts:

1) MIMX8DX5CVLFZAC

&

2) MIMX8DX5CVLDZAC

Which should be used, Not clear with the difference of FZ and DZ codes in part#.

0 Kudos
Reply

1,363 Views
igorpadykov
NXP Employee
NXP Employee

Hi Bimal

 

it is speed D-1GHz  F-1.2GHz


Best regards
igor