PMIC VGEN6 and AR8031 Sabre Current Inconsistency

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PMIC VGEN6 and AR8031 Sabre Current Inconsistency

Jump to solution
584 Views
atillametetured
Contributor V

Greetings,

The AR8031 IC on the Sabre Smart Devices is powered by VGEN6, 6th linear regulator of the PF0100. This regulator is capable of 1,8V - 3,3V voltage supply which is a check, since AR8031 nominal value is 3,3V. However, regarding the datasheet of AR8301, one can find the below table.

AR8031 Akım Çekme.PNG

As you can see the maximum current total that can be drawn by the IC is way above 200 mA, which is the maximum PF0100 is designed for. This arises the question whether if this is because it was thought the currents given on the table are improbable simultaneously or someone missed the table designing the board? This confuses me, can someone please explain why this is a valid design?

Best Regards,

Mete

Labels (3)
0 Kudos
1 Solution
449 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

acording to AR8031 datasheet p.1:

"The AR8031 requires only a single, 3.3V power

supply. On-chip regulators provide all the other

required voltages."

LX 1.1V integrated switching regulator provides power for AVDDL,DVDDL,

so power consumption AVDDL,DVDDL is included in AVDD33 consumption

(powered by VGEN6).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

2 Replies
450 Views
igorpadykov
NXP Employee
NXP Employee

Hi Atilla

acording to AR8031 datasheet p.1:

"The AR8031 requires only a single, 3.3V power

supply. On-chip regulators provide all the other

required voltages."

LX 1.1V integrated switching regulator provides power for AVDDL,DVDDL,

so power consumption AVDDL,DVDDL is included in AVDD33 consumption

(powered by VGEN6).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

449 Views
atillametetured
Contributor V

Hello Igor,

I think you are right. Thanks for you reply.

Regards,

Mete

0 Kudos