PMIC MMPF0100, how to Control VGEN5's Voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PMIC MMPF0100, how to Control VGEN5's Voltage

797件の閲覧回数
cilymo
Contributor I

HI.

   We use MMPF0100 as our board PMIC and I'm new to iMx6 platform. I want to know how to control the VGEN5 Voltage from MMPF0100. Is there any APIs to do this ?

Thanks,

Cily 

ラベル(1)
0 件の賞賛
返信
1 返信

596件の閲覧回数
art
NXP Employee
NXP Employee

From the hardware point of view, each power suppliy of the MMPF0100 PMIC, including VGEN5, is controlled by the individual set of internal registers, accessible from outside through the I2C bus. For more information, refer to the MMPF0100 Data Sheet document, available on the device's Documentation web page:

http://www.nxp.com/products/automotive-products/energy-power-management/pmics/configurable-pmics-pf-...

The latest L4.1.15 Linux BSP for the i.MX6/7 series processors also provides the driver for the MMPF0100 PMIC. For more information, refer to the Section 2.3.2 of the attached i.MX Linux Reference Manual document.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信