PF0100 coin cell charger current

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PF0100 coin cell charger current

607 次查看
emil
Contributor III

Hello,

I see in the datasheet to the PF0100 that the coin cell charger current only is 60uA. Can this be correct? That would mean that it would take 750 hours to fully charge a 45mAh coin cell battery. And at at discharge rate of 10uA I would have to keep the device on four hours a day.

Please advice.

BR,

Emil Käll

标签 (1)
标记 (1)
0 项奖励
1 回复

421 次查看
igorpadykov
NXP Employee
NXP Employee

Hi emil

document is correct, for coin cell charging one

can use external charger as well.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励