PCIe host failed to come up on Sabre SD on kernel 3.14.28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe host failed to come up on Sabre SD on kernel 3.14.28

1,676 Views
olivierlebozec
Contributor II

Hi,

I'm using SabreSD REVC4. In this version I have PCI is disabled (by default) in Uboot as stated in similar topic.

I'm using fido branch of Freescale/fsl-community-bsp-platform · GitHub

 

I got the following traces at boot with PCIe card inserted or not :

...

[ 0.386353] imx6q-pcie 1ffc000.pcie: phy link never came up
[ 0.386368] imx6q-pcie 1ffc000.pcie: Failed to bring link up!
[ 0.386396] imx6q-pcie 1ffc000.pcie: failed to initialize host
[ 0.386437] imx6q-pcie: probe of 1ffc000.pcie failed with error -22
...

 

Error comes from /drivers/pci/host/pci-imx6.c.

It seems the workarround for the missing reset wire are included in both Uboot config and in pci-imx6.c.

Any ideas to bring PCIe up?

Best regards,

Olivier.

Original Attachment has been moved to: defconfig.zip

0 Kudos
Reply
2 Replies

753 Views
olivierlebozec
Contributor II

Hi,

Using linux-fsl 3.19 and uboot-fsl solve the issue.

I think linux-imx 3.14 and uboot-imx doesn't work for PCIe. Maybe some HW initialization is missing in uboot.

My undestanding is Linux-fsl is the vanilla kernel form linux.org.

Linux-imx is the one provided by fresscale.

Am I wrong cause the name doesn"t match?

Best regards,

Olivier

0 Kudos
Reply

753 Views
igorpadykov
NXP Employee
NXP Employee

Hi Olivier

please post this to meta-fsl-arm mailing list

https://lists.yoctoproject.org/listinfo/meta-freescale

difference between Community BSP and FSL BSPs

https://community.freescale.com/message/402940#402940

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply