Hi,
I have a custom PCIe board (Gennum GN4124 + Altera Cyclone4) connected to SABRESD board with i.mx6q.
(Poky (Yocto Project Reference Distro) 1.6.1 imx6qsabresd /dev/ttymxc0)
The Gennum PCIe bridge requests 3 memory regions 1M+1M+4k, but the system does not assigned any memory.
root@imx6qsabresd:~# lspci -vv
01:00.0 Non-VGA unclassified device: Device 1a39:0004 (rev 01)
Subsystem: Device 1a39:0001
Control: I/O- Mem- BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx-
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Interrupt: pin A routed to IRQ 155
Region 0: Memory at <unassigned> (64-bit, non-prefetchable) [disabled] [size=1M]
Region 2: Memory at <unassigned> (64-bit, non-prefetchable) [disabled] [size=1M]
Region 4: Memory at <unassigned> (64-bit, non-prefetchable) [disabled] [size=4K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 NoSoftRst- PME-Enable- DSel=0 DScale=0 PME+
Capabilities: [48] MSI: Enable- Count=1/1 Maskable- 64bit+
Address: 0000000000000000 Data: 0000
Capabilities: [58] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 512 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s L1, Exit Latency L0s unlimited, L1 unlimited
ClockPM- Surprise- LLActRep- BwNot-
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- CommClk-
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis-, LTR-, OBFF Not Supported
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-, LTR-, OBFF Disabled
LnkCtl2: Target Link Speed: 2.5GT/s, EnterCompliance- SpeedDis-
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB, EqualizationComplete-, EqualizationPhase1-
EqualizationPhase2-, EqualizationPhase3-, LinkEqualizationRequest-
root@imx6qsabresd:~# dmesg | grep pci
pci_bus 0000:00: root bus resource [io 0x1000-0x10000]
pci_bus 0000:00: root bus resource [mem 0x01000000-0x01efffff]
pci_bus 0000:00: No busn resource found for root bus, will use [bus 00-ff]
pci_bus 0000:00: scanning bus
pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400
pci 0000:00:00.0: reg 10: [mem 0x00000000-0x000fffff]
pci 0000:00:00.0: reg 38: [mem 0x00000000-0x0000ffff pref]
pci 0000:00:00.0: calling pci_fixup_ide_bases+0x0/0x3c
pci 0000:00:00.0: supports D1
pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
pci 0000:00:00.0: PME# disabled
pci_bus 0000:00: fixups for bus
pci 0000:00:00.0: scanning [bus 01-01] behind bridge, pass 0
pci 0000:00:00.0: scanning [bus 00-00] behind bridge, pass 1
pci_bus 0000:01: scanning bus
pci 0000:01:00.0: [1a39:0004] type 00 class 0x000000
pci 0000:01:00.0: reg 10: [mem 0x00000000-0x000fffff 64bit]
pci 0000:01:00.0: reg 18: [mem 0x00000000-0x000fffff 64bit]
pci 0000:01:00.0: reg 20: [mem 0x00000000-0x00000fff 64bit]
pci 0000:01:00.0: calling pci_fixup_ide_bases+0x0/0x3c
pci_bus 0000:01: fixups for bus
pci_bus 0000:01: bus scan returning with max=01
pci_bus 0000:01: busn_res: [bus 01-ff] end is updated to 01
pci_bus 0000:00: bus scan returning with max=01
pci_bus 0000:00: busn_res: [bus 00-ff] end is updated to 01
pci 0000:00:00.0: fixup irq: got 155
pci 0000:00:00.0: assigning IRQ 155
pci 0000:01:00.0: fixup irq: got 155
pci 0000:01:00.0: assigning IRQ 155
pci 0000:00:00.0: BAR 0: assigned [mem 0x01000000-0x010fffff]
pci 0000:00:00.0: BAR 0: set to [mem 0x01000000-0x010fffff] (PCI address [0x1000000-0x10fffff])
pci 0000:00:00.0: BAR 8: assigned [mem 0x01100000-0x013fffff]
pci 0000:00:00.0: BAR 6: assigned [mem 0x01400000-0x0140ffff pref]
pci 0000:00:00.0: PCI bridge to [bus 01]
pci 0000:00:00.0: bridge window [mem 0x01100000-0x013fffff]
pci_bus 0000:00: resource 4 [io 0x1000-0x10000]
pci_bus 0000:00: resource 5 [mem 0x01000000-0x01efffff]
pci_bus 0000:01: resource 1 [mem 0x01100000-0x013fffff]
ehci-pci: EHCI PCI platform driver
The PCIe card works fine on a Intel Atom based embedded system.
Can someone help me in finding a solution please?
Thank you very much.
已解决! 转到解答。
Hi,
the problem is solved by setting the PCI class to 0x0680 (bridge device other).
Then the requested memory regions are assigned.
root@MBa6x:~
01:00.0 Bridge: Device 1a39:0004 (rev 01)
Subsystem: Device 1a39:0001
Control: I/O- Mem+ BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Interrupt: pin A routed to IRQ 385
Region 0: Memory at 01100000 (64-bit, non-prefetchable) [size=1M]
Region 2: Memory at 01200000 (64-bit, non-prefetchable) [size=1M]
Region 4: Memory at 01300000 (64-bit, non-prefetchable) [size=4K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [48] MSI: Mask- 64bit+ Count=4/4 Enable+
Address: 00000000472b5000 Data: 0001
Capabilities: [58] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 512 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s L1, Latency L0 unlimited, L1 unlimited
ClockPM- Surprise- LLActRep- BwNot-
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- Retrain- CommClk-
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis-
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-
LnkCtl2: Target Link Speed: 2.5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -6dB
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB
Kernel driver in use: cyclone4
in file: drivers/pci/setup-bus.c
static void __dev_sort_resources(struct pci_dev *dev, struct list_head *head)
{
u16 class = dev->class >> 8;
/* Don't touch classless devices or host bridges or ioapics. */
if (class == PCI_CLASS_NOT_DEFINED || class == PCI_CLASS_BRIDGE_HOST)
return;
/* Don't touch ioapic devices already enabled by firmware */
if (class == PCI_CLASS_SYSTEM_PIC) {
u16 command;
pci_read_config_word(dev, PCI_COMMAND, &command);
if (command & (PCI_COMMAND_IO | PCI_COMMAND_MEMORY))
return;
}
pdev_sort_resources(dev, head);
}
here my classless device missed the memory assignment.
Thanks for your help.
Gert
Hi,
the problem is solved by setting the PCI class to 0x0680 (bridge device other).
Then the requested memory regions are assigned.
root@MBa6x:~
01:00.0 Bridge: Device 1a39:0004 (rev 01)
Subsystem: Device 1a39:0001
Control: I/O- Mem+ BusMaster- SpecCycle- MemWINV- VGASnoop- ParErr+ Stepping- SERR+ FastB2B- DisINTx+
Status: Cap+ 66MHz- UDF- FastB2B- ParErr- DEVSEL=fast >TAbort- <TAbort- <MAbort- >SERR- <PERR- INTx-
Interrupt: pin A routed to IRQ 385
Region 0: Memory at 01100000 (64-bit, non-prefetchable) [size=1M]
Region 2: Memory at 01200000 (64-bit, non-prefetchable) [size=1M]
Region 4: Memory at 01300000 (64-bit, non-prefetchable) [size=4K]
Capabilities: [40] Power Management version 3
Flags: PMEClk- DSI- D1- D2- AuxCurrent=0mA PME(D0-,D1-,D2-,D3hot-,D3cold-)
Status: D0 PME-Enable- DSel=0 DScale=0 PME-
Capabilities: [48] MSI: Mask- 64bit+ Count=4/4 Enable+
Address: 00000000472b5000 Data: 0001
Capabilities: [58] Express (v2) Endpoint, MSI 00
DevCap: MaxPayload 512 bytes, PhantFunc 0, Latency L0s <64ns, L1 <1us
ExtTag- AttnBtn- AttnInd- PwrInd- RBE+ FLReset-
DevCtl: Report errors: Correctable- Non-Fatal- Fatal- Unsupported-
RlxdOrd+ ExtTag- PhantFunc- AuxPwr- NoSnoop+
MaxPayload 128 bytes, MaxReadReq 512 bytes
DevSta: CorrErr- UncorrErr- FatalErr- UnsuppReq- AuxPwr- TransPend-
LnkCap: Port #0, Speed 2.5GT/s, Width x1, ASPM L0s L1, Latency L0 unlimited, L1 unlimited
ClockPM- Surprise- LLActRep- BwNot-
LnkCtl: ASPM Disabled; RCB 64 bytes Disabled- Retrain- CommClk-
ExtSynch- ClockPM- AutWidDis- BWInt- AutBWInt-
LnkSta: Speed 2.5GT/s, Width x1, TrErr- Train- SlotClk+ DLActive- BWMgmt- ABWMgmt-
DevCap2: Completion Timeout: Range ABCD, TimeoutDis-
DevCtl2: Completion Timeout: 50us to 50ms, TimeoutDis-
LnkCtl2: Target Link Speed: 2.5GT/s, EnterCompliance- SpeedDis-, Selectable De-emphasis: -6dB
Transmit Margin: Normal Operating Range, EnterModifiedCompliance- ComplianceSOS-
Compliance De-emphasis: -6dB
LnkSta2: Current De-emphasis Level: -6dB
Kernel driver in use: cyclone4
in file: drivers/pci/setup-bus.c
static void __dev_sort_resources(struct pci_dev *dev, struct list_head *head)
{
u16 class = dev->class >> 8;
/* Don't touch classless devices or host bridges or ioapics. */
if (class == PCI_CLASS_NOT_DEFINED || class == PCI_CLASS_BRIDGE_HOST)
return;
/* Don't touch ioapic devices already enabled by firmware */
if (class == PCI_CLASS_SYSTEM_PIC) {
u16 command;
pci_read_config_word(dev, PCI_COMMAND, &command);
if (command & (PCI_COMMAND_IO | PCI_COMMAND_MEMORY))
return;
}
pdev_sort_resources(dev, head);
}
here my classless device missed the memory assignment.
Thanks for your help.
Gert