Hi,
We are trying to run different OS on different cores on sabrelite and we have a tool that partitions the resources in the device tree for these OSes.
This tool complains when there are nodes with overlapping memory regions.
e.g
At arch/arm/boot/dts/imx6qdl.dtsi there are multiple nodes that have overlapping reg properties.
Set 1:
mmdc0-1@021b0000 { /* MMDC0-1 */
compatible = “fsl,imx6q-mmdc-combine”;
};
mmdc0: mmdc@021b0000 { /* MMDC0 */
compatible = “fsl,imx6q-mmdc”;
};
Set 2:
caam_snvs: caam-snvs@020cc000 {
compatible = “fsl,imx6q-caam-snvs”;
};
snvs: snvs@020cc000 {
compatible = “fsl,sec-v4.0-mon”, “syscon”, “simple-mfd”;
};
Is this okay to have such overlaps? Do these overlaps in memory regions of different nodes in the dts indicate any problems with the DTS?
----------------
I asked this originally at https://boundarydevices.com/morty-yocto-release/#comment-376924 and was redirected here.
Thanks.
已解决! 转到解答。
Hi Abdur,
On the DTS side there is not any problem on having multiple nodes pointing to the same memory regions. An example of this use case is having 2 different drivers configuring the same module for different functionality. You may consider these use cases in your tool to get rid of those warnings/errors.
I hope this helps.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Abdur,
On the DTS side there is not any problem on having multiple nodes pointing to the same memory regions. An example of this use case is having 2 different drivers configuring the same module for different functionality. You may consider these use cases in your tool to get rid of those warnings/errors.
I hope this helps.
Regards,
Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
Just to help understanding what Adbur reports, please have a look at the NXP kernel tree imx6qdl.dtsi file:
linux-imx.git - i.MX Linux Kernel
Regards,
Gary