Optimizing power consumption in IMX platforms

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Optimizing power consumption in IMX platforms

619 次查看
lyfsci
Contributor III

Hi Experts,

Is there any white paper document on the power optimization in the iMX platforms for Linux and android ?

What are all the factors I should consider in Linux to start optimizing the power ?

Any general guidelines ?

Regards,

Lyf

标签 (2)
0 项奖励
1 回复

373 次查看
Yuri
NXP Employee
NXP Employee

Lyf,

  Please refer to section 4 (Reducing power consumption) of app note AN4509

(i.MX 6Dual/6Quad Power Consumption Measurement).

http://cache.freescale.com/files/32bit/doc/app_note/AN4509.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励