OpenGL i.mx53 on Qt 5.9.4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

OpenGL i.mx53 on Qt 5.9.4

663 次查看
alexberenshtein
Contributor III

Hi.

I make  Yocto 2.4 , with support qt 5.9.4 , with support  i.mx53qsb.

I try  run qt-opengl application . I see application is work , but opengl is no work.

What is a problem , may be  xorg , may be qt ?

Fact , accelerator is not work. 

Best regards.

0 项奖励
回复
1 回复

454 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alex

lates nxp i.MX53 official release was L2.6.35 and there is no support in

latest yocto software. Also may be useful to look on discussion on

i.MX53, Linux 4.9 and Etnaviv 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复