There are at least two versions of the i.MX6 Dual. The "DualLite" version has no GPU for OpenGL ES at all. The regular "Dual" version does have the same GC2000 GPU as the Quad and it performs similarly in my testing.
OpenGL ES 3.0 will not perform any better than OpenGL ES 2.0 unless you need some feature that is new to the 3.0 API specification. Vivante has made significant progress in improving their OpenGL ES drivers, so it's important to use the latest version regardless of whether you need 2.0 or 3.0.
Regards, Clay
The i.MX6Dual processor does not support OpenGL ES 3.0 specification at all. Only the i.MX6DualPlus and i.MX6QuadPlus processors can support it.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Artur,
Could you please reconfirm this whether OpenGL ES 3.0 is not supported dual-core?
There are test application for ES3 in opt/fsl-gpu-sdk/GLES3 folder in Yocto 2.1 FSL community BSP which makes me to think it is supported