OpenGL/ES 3.0 based on Imx6qp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OpenGL/ES 3.0 based on Imx6qp

1,878 Views
zhuchaozhu
Contributor II

Hello ,

      I encountered a problem  to transplant opengl 3.0 in imx6qp, but I would like to know whether my board supports opengl 3.0 on yotco . On yocto , opengl 2.0 runs very well in imx6qp, but i want to upgrade my software to improve imx6qp performance.

      So , I hope someone can tell me how to upgrade opengl 3.0 on the yocto platform.

Best Regards

Labels (3)
Tags (1)
0 Kudos
Reply
4 Replies

1,174 Views
zhuchaozhu
Contributor II

Hi igorpadykov

   I have downloaded Linux 4.1.15_2.0.0 BSP, and compiled through the source code. I tried to find the OpenGL-related library in the tmp directory . I  use the following command , I don't know if there are any mistakes:

   $ MACHINE=imx6qsabresd DISTRO=fsl-imx-x11 source ./fsl-setup-release.sh -b bld-x11

   $ bitbake fsl-image-gui

   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CL.so
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv2.so
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CM.so.1.1.0
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CL.so
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv2.so.2.0.0
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CL.so.1.1.0
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv2.so.2
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CL.so.1
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CL.so.1   
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CL.so.1.1.0
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CM.so.1
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CM.so
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CM.so
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLESv1_CM.so.1.1.0
   ./tmp/sysroots/imx6qsabresd/usr/lib/libGLES_CM.so.1

Thanks

0 Kudos
Reply

1,174 Views
zhuchaozhu
Contributor II

Hi igorpadykov

      Thank you for answering my question
      You suggested that I use the latest nxp bsps, but i confuse the nxp site if it is not the latest bsp.
      So I would like to confirm that Linux 4.1.15_2.0.0 BSP can support opengl 3.0 on yotco, isn't it?
      I'm looking forward for your reply.

Thanks

Linux 4.1.15_2.0.0 BSP.jpg

0 Kudos
Reply

1,174 Views
igorpadykov
NXP Employee
NXP Employee

yes Linux 4.1.15_2.0.0 BSP supports OpenGL ES3.0 as described in Release Notes

Best regards
igor

0 Kudos
Reply

1,174 Views
igorpadykov
NXP Employee
NXP Employee

Hi zhuchao

it is supported in latest nxp bsps, for example please refer to

attached Release Notes Table 9. Supported features and

use bsps described on (use Yocto Guide in doc package for installing)

http://www.nxp.com/products/software-and-tools/software-development-tools/i.mx-software-and-tools/i.... 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply