Hello I have a two part question.
1). I bitbaked the fsl-image-qt5-validation-imx for my IMX8M Quad and I have a Qt application that uses Opencv 4.4. This image builds opencv 4.2. How would I be able to upgrade to 4.4?
2). I also use "Qt5GstreamerUi-1.0, Qt5GstreamerUtils-1.0, gstreamer-1.0 and gstreamer1.0-app" packages in the application. What would I need to add to my local.conf in order to get these packages on the IMX8?
Hello rthomas,
1) yes it will work
2) For example
Add the following line to YOCTO_DIR/BUILD_DIR/conf/local.conf:
IMAGE_INSTALL_append = " qtwebkit-examples-examples"
Add the following line to YOCTO_DIR/BUILD_DIR/conf/local.conf:
IMAGE_INSTALL_append = " qtwebengine-examples"
Regards