Hi,
I have downloaded Oprofile onto ltib and tried to use the profiling tool. But I observe the following error message.
root@freescale /home/user/video_test$ opcontrol --deinit
/usr/bin/opcontrol: line 1: /usr/bin/which: No such file or directory
/usr/bin/opcontrol: line 1: /usr/bin/dirname: No such file or directory
/usr/bin/opcontrol: line 1: /ophelp: No such file or directory
I have enabled profiling support in Kernel Menu Config.
Also, I have tried downloading the source code of oprofile and compiled and attempted to use it but it still depicts the same error.
Thanks for your consideration and any help you could provide.
Regards,
Vinayak
Hi Leo,
Thanks for your suggestion. I have copied the missing files at the locations opcontrol was looking for.
But now I observe the following message on using any opcontrol command:
root@freescale ~$ opcontrol --deinit |
cpu_type 'unset' is not valid
you should upgrade oprofile or force the use of timer mode
Also, is there a way of using operf command instead of legacy opcontrol command.
Please advise.
Regards,
Vinayak
According to http://oprofile.sourceforge.net/faq/ , user-space tools are not up to date. As I can see, the latest oprofile version is 0.9.8 and what you have is 0.9.6, so you may try upgrading this package. Just download tarball and change version on the spec.
Leo
Hi,
I have installed the latest version of oprofile. Can't I use operf on this. When I attempted to use operf it gives me the following error asking me to use opcontrol instead. I have used operf on my laptop but I am not sure if it is supported on imx6.
Error:
hw perfevents: unable to reserve pmu
Unexpected error running operf: No such device
Please use the opcontrol command instead of operf
Please advise.
Regards,
Vinayak