Dear All,
I am working on IMX8QM-MEK. I needs to configure the Video preview to different degree.
Is there any register settings to change the OV5640-mipi csi Camera Version 3 Video preview to 0 deg, 90 deg and 180deg etc ?
Thanks & Regards,
Vinoth S,
vinothkumars if you found an answer, be sure to post it here. Or mark one of the answers above as correct...
Hay @vinothkumars did you find any solution for your issue? Because I am also facing the same issue .
I was trying to change the register value by
i2cget -y 3 0x3c 0x3821
i2cset -y 3 0x3c 0x3821 0x06
but nothing works in my case.
Any solution will be helpfull
Thanks and regards
Deepak Kumar Beniya
Hi,
Oh I see what you mean, well the registers will allow you to do flip and mirror only, so it gives you the ability to do 180 rotation.
However for 90 will require post-processing rotation indeed.
Regards,
Gary
Hi gary_bisson
Will you please give more information ?
Will you please share your patch ?
Thanks & Regards,
Vinoth S,
Hi,
Here is one patch I've done to have vflip/mirror read from device tree and applied during firmware download.
ov5640_mipi: allow to override vflip and mirror values · boundarydevices/linux-imx6@28d169c · GitHub
This was for an older version of the driver but it's the same, you need to make sure the fw you download when switching resolution doesn't get overwritten.
Regards,
Gary
Hi gary_bisson
Do you know is there any other hardware register able to rotate OV5640 view ?
Thanks & Regards,
Vinoth S,
Hi Vinoth,
You should look at the datasheet of the sensor:
https://cdn.sparkfun.com/datasheets/Sensors/LightImaging/OV5640_datasheet.pdf
You'll see the following section that replies to your question (avoids doing a transform in user-space, hence better):
Regards,
Gary
Thank you gary_bisson,
I already configured and test with these register but, I am unable rotate this view
0x3820 & 0x3821
Do you know any configuration/ register to rotate the preview ?
Regards,
Vinoth S,
Hi,
It means you are overwriting the value at some point. Because I've used those registers before and they work ok.
I suggest you read back those registers during the preview to make sure they are properly set.
Regards,
Gary
In my experience, I haven't found a way to change the video rotation in a hardware register. In software it can be done using gstreamer and the videoflip pipeline element. If you would like to render the video stream in an app (in my case, a Qt app) you can create a gstreamer pipeline and poll it for an image, store the image buffer into a QImage, and then use the QImage::mirrored or QImage::transformed functions. This is useful if, for instance, you want to do some sort of compute on the un-flipped video image but want to render the flipped one for users. Doing this on the i.MX8QXP, we ran into performance issues if the frame rate was too high, but I'm pretty sure the i.MX8QM has better video capabilities.
Hope that helps!
Nolan Z
Thank You nolan.zinn@bayer.com for the reply.
I am working on Android 9 Automotive with Rear View Camera functionality (SDK_MEK-MIMX8QM). Do you know about flip mechanism ?
This is what observation. If you know any configuration let me the regarding orientation.
Regards,
Vinoth S,
With gstreamer you would use a (c++) command like this:
const char* launchCmd = "/dev/video1 " +
"! video/x-raw,width=1920,height=1080 " +
"! videoflip method=counterclockwise " +
"! autovideoconvert " +
"! video/x-raw,format=RGB16 " +
"! appsink name=\"mysink\"";
GError *error = null;
GstElement *pipeline = gst_parse_launch(launchCmd, &error);
The Java api for gstreamer is located at gstreamer-java · GitHub .
Nolan Z