We develop one i.MX53 board which integrated OV3640 CMOS image sensor connected with CSI0 port. And get the driver from the L2.6.35_11.09.01_ER_source_bundle.tar.gz package. OV3640 works but the image is bad in color.
I inputed the gstreamer command line as followings:
gst-launch -v mfw_v4lsrc capture-width=640 capture-height=480 ! mfw_v4lsink
I recorded the video on the screen using my mobile phone and attached. The image's shape was clear but the color was bad. The colorful bar was flickering and shinning. Whether I have some mistake on the color format?
Can anybody help me for this problem? Thank you!
I made a board and connected the typical ebay OV3640 module, modprobe does not give any errors and seems to load the kernel modules but can't open /dev/video0. How does the driver know which I2C bus is used to probe the module?