OTA upgrade from Nougat to Oreo

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OTA upgrade from Nougat to Oreo

926 Views
sumankumar
Contributor I

Hi,

How do i flash GPT image during OTA update?

We have devices in the field running Nougat (7.1.1) on imx6 and want to upgrade to Oreo.

For development, we have used 'fastboot flash gpt oreo-gpt.img" through USB and our system works fine.

We now want to rollout the upgrade to devices in the field.

The FSLOta.apk downloads the ota package to cache partition but how do i re-partition the eMMC for Oreo partition sizes and then apply the OTA upgrade?

Labels (2)
Tags (4)
0 Kudos
Reply
1 Reply

806 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

Please take a look to the Android Frequently Asked Questions attached,

Chapter 32 How do I customize the reference OTA application?

 

Hope this helps,

Best regards, 
Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply