Generating continuous frame clock on SAI interface of iMX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generating continuous frame clock on SAI interface of iMX8M

2,136 Views
ani10c89
Contributor II

Hi,

We are using SAI3 interface of iMX8M to connect to Audio transceiver. Audio transceiver has requirement of continuous Frame Sync clock (TXFS) on I2S interface. Can you please let us know how to get continuous clock on TXFS pin of SAI3 interface in iMX8M.

Regards,

Anirudha

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

2,029 Views
markruthenbeck
NXP Employee
NXP Employee

Anirudha,

Is there a problem with the SAI or are you asking a "how to" question?

mark

0 Kudos
Reply

2,029 Views
ani10c89
Contributor II

Hi Mark,

I am asking How to generate continuous clock on Frame Sync Signal on SAI3.

Regards,

Anirudha

0 Kudos
Reply

2,029 Views
markruthenbeck
NXP Employee
NXP Employee

Aniruda,

I am still not quite clear on the question. when the 8M is the master, the clock and frame sync are operational when the device is xmitting data. as soon as the data stops, the clocks also stop.

to keep the clocks running, you will need to xmit something like a "digital mute" which would be just zeros.

thanks,

mark

0 Kudos
Reply