No soundcards found in ALSA device list

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No soundcards found in ALSA device list

Jump to solution
2,044 Views
simonlin
Contributor II

Hi  NXP

Here's my environment

SoC:imx8qm

audio chip:add2010

OS:yocto kirkstone

Linux version:5.15.71

It show No soundcards found in ALSA device list

But I cat /proc/asound/cards, the add2010 audio is registered successful

I try to play audio file, and control audio volume are OK

I don't understand why it show No soundcards found in boot log


Booting from mmc ...
106496 bytes read in 2 ms (50.8 MiB/s)
Loading hdp firmware from 0x000000009c000000 offset 0x0000000000002000
Loading hdp firmware Complete
129532 bytes read in 2 ms (61.8 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
ERROR: reserving fdt memory region failed (addr=90400000 size=100000 flags=4)
ERROR: reserving fdt memory region failed (addr=901ff000 size=1000 flags=4)
Using Device Tree in place at 0000000083000000, end 00000000830229fb
Disable pwm@5a190000 rsrc 188 not owned
Disable clock-controller@5a590000 rsrc 188 not owned
Disable jr@40000 rsrc 502 not owned

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000100 [0x410fd082]
[ 0.000000] Linux version 5.15.71+ga753ba3716b0 (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.3.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Tue May 7 08:45:30 UTC 2024
[ 0.000000] Machine model: Freescale i.MX8QM CNH Pegasus
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 960 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000090400000, size 1 MiB
[ 0.000000] OF: reserved mem: initialized node vdevbuffer, compatible id shared-dma-pool
[ 0.000000] earlycon: lpuart32 at MMIO32 0x000000005a060000 (options '')
[ 0.000000] printk: bootconsole [lpuart32] enabled
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000080200000-0x00000009ffffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x9feffe800-0x9ff000fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000080200000-0x00000000ffffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal [mem 0x0000000100000000-0x00000009ffffffff]
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000080200000-0x0000000083ffffff]
[ 0.000000] node 0: [mem 0x0000000084000000-0x00000000863fffff]
[ 0.000000] node 0: [mem 0x0000000086400000-0x000000008fffffff]
[ 0.000000] node 0: [mem 0x0000000090000000-0x000000009001ffff]
[ 0.000000] node 0: [mem 0x0000000090020000-0x00000000900fefff]
[ 0.000000] node 0: [mem 0x00000000900ff000-0x000000009011ffff]
[ 0.000000] node 0: [mem 0x0000000090120000-0x00000000901fefff]
[ 0.000000] node 0: [mem 0x00000000901ff000-0x00000000901fffff]
[ 0.000000] node 0: [mem 0x0000000090200000-0x00000000903fffff]
[ 0.000000] node 0: [mem 0x0000000090400000-0x00000000904fffff]
[ 0.000000] node 0: [mem 0x0000000090500000-0x0000000091ffffff]
[ 0.000000] node 0: [mem 0x0000000092000000-0x00000000920fffff]
[ 0.000000] node 0: [mem 0x0000000092100000-0x00000000943fffff]
[ 0.000000] node 0: [mem 0x0000000094400000-0x00000000951fffff]
[ 0.000000] node 0: [mem 0x0000000095200000-0x00000000fdffffff]
[ 0.000000] node 0: [mem 0x0000000880000000-0x000000088fffffff]
[ 0.000000] node 0: [mem 0x0000000890000000-0x00000009ffffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000080200000-0x00000009ffffffff]
[ 0.000000] On node 0, zone DMA: 512 pages in unavailable ranges
[ 0.000000] On node 0, zone Normal: 8192 pages in unavailable ranges
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s41368 r8192 d32360 u81920
[ 0.000000] Detected PIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: Spectre-v2
[ 0.000000] CPU features: detected: Spectre-v3a
[ 0.000000] CPU features: detected: Spectre-BHB
[ 0.000000] CPU features: detected: ARM errata 1165522, 1319367, or 1530923
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 2055688
[ 0.000000] Policy zone: Normal
[ 0.000000] Kernel command line: console=ttyLP0,115200 earlycon root=/dev/mmcblk0p2 rootwait rw cpufreq.default_governor=SCHEDUTIL
[ 0.000000] Dentry cache hash table entries: 1048576 (order: 11, 8388608 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] software IO TLB: mapped [mem 0x00000000bc000000-0x00000000c0000000] (64MB)
[ 0.000000] Memory: 6667276K/8353792K available (17856K kernel code, 1530K rwdata, 7052K rodata, 2944K init, 534K bss, 703476K reserved, 983040K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=6, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=6.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=6
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 512 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 100 region 0:0x0000000051b80000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.008371] Console: colour dummy device 80x25
[ 0.012523] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.022730] pid_max: default: 32768 minimum: 301
[ 0.027361] LSM: Security Framework initializing
[ 0.032020] Mount-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.039534] Mountpoint-cache hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.048501] rcu: Hierarchical SRCU implementation.
[ 0.054088] EFI services will not be available.
[ 0.058553] smp: Bringing up secondary CPUs ...
[ 0.064497] CPU features: detected: ARM erratum 845719
[ 0.064520] Detected VIPT I-cache on CPU1
[ 0.064556] GICv3: CPU1: found redistributor 0 region 0:0x0000000051b00000
[ 0.064615] CPU1: Booted secondary processor 0x0000000000 [0x410fd034]
[ 0.065506] Detected VIPT I-cache on CPU2
[ 0.065523] GICv3: CPU2: found redistributor 1 region 0:0x0000000051b20000
[ 0.065546] CPU2: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.066360] Detected VIPT I-cache on CPU3
[ 0.066378] GICv3: CPU3: found redistributor 2 region 0:0x0000000051b40000
[ 0.066401] CPU3: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.067217] Detected VIPT I-cache on CPU4
[ 0.067235] GICv3: CPU4: found redistributor 3 region 0:0x0000000051b60000
[ 0.067258] CPU4: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.068075] Detected PIPT I-cache on CPU5
[ 0.068095] GICv3: CPU5: found redistributor 101 region 0:0x0000000051ba0000
[ 0.068118] CPU5: Booted secondary processor 0x0000000101 [0x410fd082]
[ 0.068165] smp: Brought up 1 node, 6 CPUs
[ 0.164104] SMP: Total of 6 processors activated.
[ 0.168790] CPU features: detected: 32-bit EL0 Support
[ 0.173920] CPU features: detected: 32-bit EL1 Support
[ 0.179040] CPU features: detected: CRC32 instructions
[ 0.200003] CPU: All CPU(s) started at EL2
[ 0.203798] alternatives: patching kernel code
[ 0.209125] devtmpfs: initialized
[ 0.219973] KASLR disabled due to lack of seed
[ 0.224182] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.233816] futex hash table entries: 2048 (order: 5, 131072 bytes, linear)
[ 0.250911] pinctrl core: initialized pinctrl subsystem
[ 0.256148] DMI not present or invalid.
[ 0.259968] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.268601] DMA: preallocated 1024 KiB GFP_KERNEL pool for atomic allocations
[ 0.275778] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.283690] DMA: preallocated 1024 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.291395] audit: initializing netlink subsys (disabled)
[ 0.296860] audit: type=2000 audit(0.184:1): state=initialized audit_enabled=0 res=1
[ 0.297154] thermal_sys: Registered thermal governor 'step_wise'
[ 0.304475] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.310820] cpuidle: using governor menu
[ 0.321037] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.327783] ASID allocator initialised with 65536 entries
[ 0.333868] Serial: AMBA PL011 UART driver
[ 0.337663] imx mu driver is registered.
[ 0.341535] imx rpmsg driver is registered.
[ 0.377225] platform bus@56240000:ldb@562410e0: Fixing up cyclic dependency with 56180000.dpu
[ 0.388074] platform 56228000.dsi_host: Fixing up cyclic dependency with 56180000.dpu
[ 0.397864] platform lvds1_panel: Fixing up cyclic dependency with bus@56240000:ldb@562410e0
[ 0.413542] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.419911] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.426590] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.433278] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.440922] cryptd: max_cpu_qlen set to 1000
[ 0.448091] ACPI: Interpreter disabled.
[ 0.452467] iommu: Default domain type: Translated
[ 0.457052] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.463418] vgaarb: loaded
[ 0.466098] SCSI subsystem initialized
[ 0.469903] usbcore: registered new interface driver usbfs
[ 0.475182] usbcore: registered new interface driver hub
[ 0.480475] usbcore: registered new device driver usb
[ 0.486766] mc: Linux media interface: v0.10
[ 0.490718] videodev: Linux video capture interface: v2.00
[ 0.496207] pps_core: LinuxPPS API ver. 1 registered
[ 0.501120] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.510245] PTP clock support registered
[ 0.514169] EDAC MC: Ver: 3.0.0
[ 0.518647] FPGA manager framework
[ 0.521747] --> alsa_sound_init
[ 0.524835] --> snd_minor_info_init
[ 0.528309] --> snd_card_info_init
[ 0.531690]
[ 0.533168] Advanced Linux Sound Architecture Driver Initialized.
[ 0.539516] Bluetooth: Core ver 2.22
[ 0.542823] NET: Registered PF_BLUETOOTH protocol family
[ 0.548112] Bluetooth: HCI device and connection manager initialized
[ 0.554454] Bluetooth: HCI socket layer initialized
[ 0.559318] Bluetooth: L2CAP socket layer initialized
[ 0.564364] Bluetooth: SCO socket layer initialized
[ 0.570016] imx-scu scu: NXP i.MX SCU Initialized
[ 0.590389] imx8qm-pinctrl scu:pinctrl: initialized IMX pinctrl driver
[ 0.598277] clocksource: Switched to clocksource arch_sys_counter
[ 0.604151] VFS: Disk quotas dquot_6.6.0
[ 0.607980] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.614899] pnp: PnP ACPI: disabled
[ 0.644440] NET: Registered PF_INET protocol family
[ 0.649370] IP idents hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.658667] tcp_listen_portaddr_hash hash table entries: 4096 (order: 4, 65536 bytes, linear)
[ 0.666907] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[ 0.674594] TCP established hash table entries: 65536 (order: 7, 524288 bytes, linear)
[ 0.682758] TCP bind hash table entries: 65536 (order: 8, 1048576 bytes, linear)
[ 0.690393] TCP: Hash tables configured (established 65536 bind 65536)
[ 0.696691] UDP hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 0.703460] UDP-Lite hash table entries: 4096 (order: 5, 131072 bytes, linear)
[ 0.710759] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.716549] RPC: Registered named UNIX socket transport module.
[ 0.722129] RPC: Registered udp transport module.
[ 0.726829] RPC: Registered tcp transport module.
[ 0.731504] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.737940] PCI: CLS 0 bytes, default 64
[ 0.742483] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available
[ 0.750779] kvm [1]: IPA Size Limit: 40 bits
[ 0.755340] kvm [1]: vgic-v2@52020000
[ 0.758684] kvm [1]: GIC system register CPU interface enabled
[ 0.764609] kvm [1]: vgic interrupt IRQ9
[ 0.768531] kvm [1]: Hyp mode initialized successfully
[ 0.776542] workingset: timestamp_bits=42 max_order=21 bucket_order=0
[ 0.785471] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.791314] NFS: Registering the id_resolver key type
[ 0.796042] Key type id_resolver registered
[ 0.800190] Key type id_legacy registered
[ 0.804222] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.810877] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.818272] jffs2: version 2.2. (NAND) c 2001-2006 Red Hat, Inc.
[ 0.824534] 9p: Installing v9fs 9p2000 file system support
[ 0.854265] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.861333] io scheduler mq-deadline registered
[ 0.865848] io scheduler kyber registered
[ 0.881394] EINJ: ACPI disabled.
[ 1.054147] mxs-dma 5b810000.dma-apbh: initialized
[ 1.061687] Bus freq driver module loaded
[ 1.070643] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 1.079220] 5a060000.serial: ttyLP0 at MMIO 0x5a060010 (irq = 58, base_baud = 5000000) is a FSL_LPUAR[ 1.088376] printk: console [ttyLP0] enabled
[ 1.088376] printk: console [ttyLP0] enabled
[ 1.096801] printk: bootconsole [lpuart32] disabled
[ 1.096801] printk: bootconsole [lpuart32] disabled
[ 1.107010] 5a080000.serial: ttyLP2 at MMIO 0x5a080010 (irq = 59, base_baud = 5000000) is a FSL_LPUART
[ 1.116824] 5a090000.serial: ttyLP3 at MMIO 0x5a090010 (irq = 60, base_baud = 5000000) is a FSL_LPUART
[ 1.126772] 5a0a0000.serial: ttyLP4 at MMIO 0x5a0a0010 (irq = 85, base_baud = 5000000) is a FSL_LPUART
[ 1.137630] arm-smmu 51400000.iommu: probing hardware configuration...
[ 1.144183] arm-smmu 51400000.iommu: SMMUv2 with:
[ 1.148891] arm-smmu 51400000.iommu: stage 1 translation
[ 1.154293] arm-smmu 51400000.iommu: stage 2 translation
[ 1.159697] arm-smmu 51400000.iommu: nested translation
[ 1.165014] arm-smmu 51400000.iommu: stream matching with 32 register groups
[ 1.172159] arm-smmu 51400000.iommu: 32 context banks (0 stage-2 only)
[ 1.178781] arm-smmu 51400000.iommu: Supported page sizes: 0x61311000
[ 1.185308] arm-smmu 51400000.iommu: Stage-1: 48-bit VA -> 48-bit IPA
[ 1.191841] arm-smmu 51400000.iommu: Stage-2: 48-bit IPA -> 48-bit PA
[ 1.198437] arm-smmu 51400000.iommu: preserved 0 boot mappings
[ 1.283399] loop: module loaded
[ 1.288345] of_reserved_mem_lookup() returned NULL
[ 1.293207] megasas: 07.717.02.00-rc1
[ 1.299118] imx ahci driver is registered.
[ 1.311195] tun: Universal TUN/TAP device driver, 1.6
[ 1.316392] CAN device driver interface
[ 1.323928] thunder_xcv, ver 1.0
[ 1.327204] thunder_bgx, ver 1.0
[ 1.330457] nicpf, ver 1.0
[ 1.336837] hclge is initializing
[ 1.340194] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.347424] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.352798] e1000: Intel(R) PRO/1000 Network Driver
[ 1.357680] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.363447] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.368471] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.374418] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.379822] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.385442] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.391719] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.398039] sky2: driver version 1.30
[ 1.402813] usbcore: registered new interface driver r8152
[ 1.408488] VFIO - User Level meta-driver version: 0.3
[ 1.417102] cdns3-imx 5b110000.usb: Adding to iommu group 0
[ 1.424242] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.430801] ehci-pci: EHCI PCI platform driver
[ 1.435304] ehci-platform: EHCI generic platform driver
[ 1.441030] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.447229] ohci-pci: OHCI PCI platform driver
[ 1.451707] ohci-platform: OHCI generic platform driver
[ 1.458013] usbcore: registered new interface driver uas
[ 1.463369] usbcore: registered new interface driver usb-storage
[ 1.469428] usbcore: registered new interface driver usbserial_generic
[ 1.475967] usbserial: USB Serial support registered for generic
[ 1.481991] usbcore: registered new interface driver ftdi_sio
[ 1.487791] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.495142] usbcore: registered new interface driver usb_serial_simple
[ 1.501682] usbserial: USB Serial support registered for carelink
[ 1.507792] usbserial: USB Serial support registered for zio
[ 1.513463] usbserial: USB Serial support registered for funsoft
[ 1.519483] usbserial: USB Serial support registered for flashloader
[ 1.525851] usbserial: USB Serial support registered for google
[ 1.531791] usbserial: USB Serial support registered for libtransistor
[ 1.538336] usbserial: USB Serial support registered for vivopay
[ 1.544356] usbserial: USB Serial support registered for moto_modem
[ 1.550637] usbserial: USB Serial support registered for motorola_tetra
[ 1.557314] usbserial: USB Serial support registered for nokia
[ 1.563247] usbserial: USB Serial support registered for novatel_gps
[ 1.569697] usbserial: USB Serial support registered for hp4x
[ 1.575526] usbserial: USB Serial support registered for suunto
[ 1.581486] usbserial: USB Serial support registered for siemens_mpi
[ 1.587920] usbcore: registered new interface driver usb_ehset_test
[ 1.601722] input: sc-powerkey as /devices/platform/sc-powerkey/input/input0
[ 1.609432] i2c_dev: i2c /dev entries driver
[ 1.621750] amphion-vpu-core 2d080000.vpu-core: [0] = decoder
[ 1.629359] amphion-vpu-core 2d090000.vpu-core: [1] = encoder
[ 1.637302] amphion-vpu-core 2d0a0000.vpu-core: [2] = encoder
[ 1.650649] Bluetooth: HCI UART driver ver 2.3
[ 1.655112] Bluetooth: HCI UART protocol H4 registered
[ 1.660253] Bluetooth: HCI UART protocol BCSP registered
[ 1.665583] Bluetooth: HCI UART protocol LL registered
[ 1.670724] Bluetooth: HCI UART protocol ATH3K registered
[ 1.676134] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.682638] Bluetooth: HCI UART protocol Broadcom registered
[ 1.688308] Bluetooth: HCI UART protocol QCA registered
[ 1.697268] sdhci: Secure Digital Host Controller Interface driver
[ 1.703488] sdhci: Copyright(c) Pierre Ossman
[ 1.709116] Synopsys Designware Multimedia Card Interface Driver
[ 1.716387] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.724729] sdhci-esdhc-imx 5b010000.mmc: Adding to iommu group 1
[ 1.731030] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.738653] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.745198] usbcore: registered new interface driver usbhid
[ 1.750780] usbhid: USB HID core driver
[ 1.756850] mxc-isi 58100000.isi: mxc_isi.0 registered successfully
[ 1.763684] mxc-isi 58110000.isi: mxc_isi.1 registered successfully
[ 1.764207] mmc0: SDHCI controller on 5b010000.mmc [5b010000.mmc] using ADMA
[ 1.770546] mxc-isi 58120000.isi: mxc_isi.2 registered successfully
[ 1.783868] mxc-isi 58130000.isi: mxc_isi.3 registered successfully
[ 1.798590] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.807502] optee: probing for conduit method.
[ 1.811975] optee: revision 3.19 (00919403)
[ 1.812620] optee: initialized driver
[ 1.825278] Galcore version 6.4.3.p4.398061
[ 1.832264] mmc0: new HS400 Enhanced strobe MMC card at address 0001
[ 1.839290] mmcblk0: mmc0:0001 AAM20F 59.3 GiB
[ 1.842541] [drm] Initialized vivante 1.0.0 20170808 for 80000000.imx8_gpu1_ss on minor 0
[ 1.852201] mmcblk0: p1 p2
[ 1.855070] --> snd_register_device
[ 1.855549] mmcblk0boot0: mmc0:0001 AAM20F 31.5 MiB
[ 1.861427] NET: Registered PF_LLC protocol family
[ 1.864797] mmcblk0boot1: mmc0:0001 AAM20F 31.5 MiB
[ 1.868670] NET: Registered PF_INET6 protocol family
[ 1.874384] mmcblk0rpmb: mmc0:0001 AAM20F 4.00 MiB, chardev (234:0)
[ 1.878761] Segment Routing with IPv6
[ 1.888262] In-situ OAM (IOAM) with IPv6
[ 1.892220] NET: Registered PF_PACKET protocol family
[ 1.897296] can: controller area network core
[ 1.901683] NET: Registered PF_CAN protocol family
[ 1.906490] can: raw protocol
[ 1.909467] can: broadcast manager protocol
[ 1.913659] can: netlink gateway - max_hops=1
[ 1.918139] Bluetooth: RFCOMM TTY layer initialized
[ 1.923023] Bluetooth: RFCOMM socket layer initialized
[ 1.928192] Bluetooth: RFCOMM ver 1.11
[ 1.931953] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.937264] Bluetooth: BNEP filters: protocol multicast
[ 1.942510] Bluetooth: BNEP socket layer initialized
[ 1.947495] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.953419] Bluetooth: HIDP socket layer initialized
[ 1.958486] 8021q: 802.1Q VLAN Support v1.8
[ 1.962689] lib80211: common routines for IEEE802.11 drivers
[ 1.968411] 9pnet: Installing 9P2000 support
[ 1.972705] tsn generic netlink module v1 init...
[ 1.977449] Key type dns_resolver registered
[ 2.000893] mxs_phy 5b100000.usbphy: supply phy-3p0 not found, using dummy regulator
[ 2.022823] imx-lpi2c 58226000.i2c: use pio mode
[ 2.027819] i2c 2-0044: Fixing up cyclic dependency with 58227000.csi
[ 2.058451] isl7998x 2-0044: isl7998x_write_reg:write reg error:reg=ff,val= 0
[ 2.066060] isl7998x 2-0044: In isl7998x_hardware_init()
[ 2.090352] isl7998x 2-0044: isl7998x_data->num_lanes=2
[ 2.131416] isl7998x 2-0044: isl7998x is found, id = 0x87, name isl7998x 2-0044
[ 2.138890] i2c i2c-2: LPI2C adapter registered
[ 2.144390] gpio-430 (scl): enforced open drain please flag it properly in DT/ACPI DSDT/board file
[ 2.153380] imx-lpi2c 5a810000.i2c: using scl,sda for recovery
[ 2.159228] imx-lpi2c 5a810000.i2c: use pio mode
[ 2.167555] hwmon hwmon6: temp1_input not attached to any thermal zone
[ 2.174106] lm75 3-0048: hwmon6: sensor 'tmp75'
[ 2.179289] elan_ktf 3-0016: [elan] enter elants_i2c_probe...v.0.0.14-17
[ 2.182139] rtc-ds1307 3-0068: registered as rtc0
[ 2.186283] elan_ktf 3-0016: supply vcc33 not found, using dummy regulator
[ 2.191036] rtc-ds1307 3-0068: setting system clock to 2000-01-20T17:52:57 UTC (948390777)
[ 2.197916] elan_ktf 3-0016: supply vccio not found, using dummy regulator
[ 2.206024] i2c 3-0051: Fixing up cyclic dependency with 5b130000.usb
[ 2.213111] elan_ktf 3-0016: [elan] ts->intr_gpio = 310.
[ 2.224835] elan_ktf 3-0016: [elan] irq num = 459.
[ 2.229653] elan_ktf 3-0016: Power_on
[ 2.230183] i2c i2c-3: LPI2C adapter registered
[ 2.239058] imx-lpi2c 5a830000.i2c: use pio mode
[ 2.244242] msi-mcu 4-0020: ++ mcu_probe ++ << i2c_device_probe
[ 2.250212] msi-mcu 4-0020: got channel select gpio.
[ 2.255194] msi-mcu 4-0020: create file ok: 0
[ 2.259562] msi-mcu 4-0020: create file ok: 0
[ 2.263932] msi-mcu 4-0020: create file ok: 0
[ 2.268302] msi-mcu 4-0020: create file ok: 0
[ 2.272746] msi-mcu 4-0020: register backlight pwm, 0
[ 2.277855] msi-mcu 4-0020: == init_rgb_pwm == register led: 0
[ 2.283741] msi-mcu 4-0020: == init_rgb_pwm == register led: 0
[ 2.289623] msi-mcu 4-0020: == init_rgb_pwm == register led: 0
[ 2.295465] msi-mcu 4-0020: == init_runtime_cvbs_input == create file ok: 0
[ 2.302439] msi-mcu 4-0020: ++ init_wakeup_source ++ got IRQ 398
[ 2.308749] msi-mcu 4-0020: -- init_wakeup_source -- request irq: 0
[ 2.315111] msi-mcu 4-0020: -- mcu_probe --
[ 2.319722] ms5629-adc 4-0021: ms5629-adc, dev_info
[ 2.325029] at24 4-0056: supply vcc not found, using dummy regulator
[ 2.332117] at24 4-0056: read 1@0 --> 0 (4294892826)
[ 2.337122] at24 4-0056: 1024 byte br24g64 EEPROM, writable, 32 bytes/write
[ 2.362888] random: crng init done
[ 2.369007] shx goin add2010_probe start
[ 2.373110] client->addr = 0x30
[ 2.376346] add2010 4-0030: supply dvdd not found, using dummy regulator
[ 2.383124] add2010 4-0030: supply pvdd not found, using dummy regulator
[ 2.390309] devm_snd_soc_register_component ret = 0
[ 2.395206] shx goin add2010_probe end
[ 2.399602] add2010 chip_id = 0xc8
[ 2.403077] i2c i2c-4: LPI2C adapter registered
[ 2.411355] pwm-backlight lvds_backlight@0: supply power not found, using dummy regulator
[ 2.421028] pwm-backlight lvds_backlight@1: supply power not found, using dummy regulator
[ 2.438492] dpu-core 56180000.dpu: driver probed
[ 2.445060] dpu-core 57180000.dpu: driver probed
[ 2.546467] [elan] enter elants_i2c_initialize....
[ 2.554179] elan_ktf 3-0016: 43 00 02 01 20 ff ff ff
[ 2.559153] elan_ktf 3-0016: ff ff ff ff ff ff ff ff
[ 2.564119] elan_ktf 3-0016: ff ff ff ff ff ff ff ff
[ 2.569090] elan_ktf 3-0016: ff ff ff ff ff ff ff ff
[ 2.574062] elan_ktf 3-0016: ff ff ff ff ff ff ff ff
[ 2.579027] elan_ktf 3-0016: [elan] Johnny: Receive 0x20, Gen7, in Normal Mode.
[ 2.589105] elan_ktf 3-0016: [elan] elants_i2c_query_hw_version: (Firmware ID) 43 00 02 04 52 f4 33 01
[ 2.601083] elan_ktf 3-0016: [elan] elants_i2c_query_bc_version: (BC version) 43 00 02 04 52 19 c0 81
[ 2.613268] elan_ktf 3-0016: [elan] elants_i2c_query_fw_version: (Firmware version) 43 00 02 04 52 08 30 81
[ 2.625744] elan_ktf 3-0016: [elan] elants_i2c_query_test_version: (test version) 43 00 02 04 52 e0 00 04
[ 2.638006] elan_ktf 3-0016: [elan] elants_i2c_query_ts_info: (get resolution) 43 00 02 11 9b 2c 32 1c
[ 2.650002] elan_ktf 3-0016: [elan] elants_i2c_query_ts_info: (get osr) 43 00 02 04 52 d6 00 30
[ 2.661456] elan_ktf 3-0016: [elan] elants_i2c_query_ts_info: (get physical scan) 43 00 02 04 52 d7 01 26
[ 2.673682] elan_ktf 3-0016: [elan] elants_i2c_query_ts_info: ts->cols=28, ts->rows=50, x_max=2352, x_res=8, y_max=1296, y_res=8
[ 2.685268] elan_ktf 3-0016: [elan]init delayed work for elants_auto_update
[ 2.692451] input: Elan Touchscreen as /devices/platform/bus@5a000000/5a810000.i2c/i2c-3/3-0016/input/input1
[ 2.702366] elan_ktf 3-0016: set irqflags = IRQF_TRIGGER_LOW
[ 2.708229] elan_ktf 3-0016: [elan] misc_register finished!!
[ 2.911719] tcan4x5x spi0.0: m_can device registered (irq=405, version=32)
[ 2.918610] tcan4x5x spi0.0 can3: TCAN4X5X successfully initialized.
[ 2.925739] fec 5b040000.ethernet: Adding to iommu group 2
[ 3.038889] pps pps0: new PPS source ptp0
[ 3.043774] fec 5b040000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 3.050820] fec 5b040000.ethernet: Using random MAC address: e2:cb:df:79:36:f1
[ 3.060404] fec 5b040000.ethernet eth0: registered PHC device 0
[ 3.067430] fec 5b050000.ethernet: Adding to iommu group 2
[ 3.178755] pps pps1: new PPS source ptp1
[ 3.183648] fec 5b050000.ethernet: Invalid MAC address: 00:00:00:00:00:00
[ 3.190752] fec 5b050000.ethernet: Using random MAC address: 3a:87:9a:fe:28:7f
[ 3.200944] fec 5b050000.ethernet eth1: registered PHC device 1
[ 3.207910] cdns-usb3 5b130000.usb: Adding to iommu group 0
[ 3.215033] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.220554] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 1
[ 3.229032] xhci-hcd xhci-hcd.1.auto: hcc params 0x200073c8 hci version 0x100 quirks 0x0000002200018010
[ 3.238488] xhci-hcd xhci-hcd.1.auto: irq 237, io mem 0x5b130000
[ 3.244882] xhci-hcd xhci-hcd.1.auto: xHCI Host Controller
[ 3.250390] xhci-hcd xhci-hcd.1.auto: new USB bus registered, assigned bus number 2
[ 3.258077] xhci-hcd xhci-hcd.1.auto: Host supports USB 3.0 SuperSpeed
[ 3.265249] hub 1-0:1.0: USB hub found
[ 3.269036] hub 1-0:1.0: 1 port detected
[ 3.273163] usb usb2: We don't know the algorithms for LPM for this host, disabling LPM.
[ 3.281510] hub 2-0:1.0: USB hub found
[ 3.285290] hub 2-0:1.0: 1 port detected
[ 3.293450] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 3.298365] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 3
[ 3.318297] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 3.324045] hub 3-0:1.0: USB hub found
[ 3.327828] hub 3-0:1.0: 1 port detected
[ 3.354289] mxc-mipi-csi2 58227000.csi: lanes: 2, name: mxc-mipi-csi2.0
[ 3.366730] xhci-hcd xhci-hcd.1.auto: remove, state 1
[ 3.371813] usb usb2: USB disconnect, device number 1
[ 3.377292] xhci-hcd xhci-hcd.1.auto: USB bus 2 deregistered
[ 3.383032] xhci-hcd xhci-hcd.1.auto: remove, state 84
[ 3.388176] usb usb1: USB disconnect, device number 1
[ 3.399880] xhci-hcd xhci-hcd.1.auto: USB bus 1 deregistered
[ 3.409619] imx-lpi2c 56226000.i2c: use pio mode
[ 3.414527] i2c 5-0062: Fixing up cyclic dependency with external_panel
[ 3.421179] i2c 5-0062: Fixing up cyclic dependency with 56228000.dsi_host
[ 3.428338] max96789 5-0062: max96789_probe : max96789_probe start
[ 3.434524] max96789_probe : max96789_probe start
[ 3.464484] max96789 5-0062: drm_of_find_panel_or_bridge(dev->of_node, 2, 0, &panel, &panel_bridge) fail
[ 3.473977] max96789 5-0062: max96789_probe : max96789_parse_dt fail
[ 3.480462] i2c i2c-5: LPI2C adapter registered
[ 3.485855] panel-simple external_panel: Specify missing connector_type
[ 3.486040] imx6q-pcie 5f000000.pcie: supply epdev_on not found, using dummy regulator
[ 3.493940] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.500826] imx6q-pcie 5f000000.pcie: No cache used with register defaults set!
[ 3.508795] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[ 3.524367] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.531891] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.539437] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[ 3.542289] imx6q-pcie 5f000000.pcie: PCIe PLL is locked.
[ 3.547111] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[ 3.552229] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[ 3.564922] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 3.572514] imx6q-pcie 5f000000.pcie: host bridge /bus@5f000000/pcie@0x5f000000 ranges:
[ 3.580576] imx6q-pcie 5f000000.pcie: IO 0x006ff80000..0x006ff8ffff -> 0x0000000000
[ 3.588790] usb 3-1: new high-speed USB device number 2 using ci_hdrc
[ 3.595277] imx6q-pcie 5f000000.pcie: MEM 0x0060000000..0x006fefffff -> 0x0060000000
[ 3.596142] imx-drm display-subsystem: bound bus@56240000:ldb@562410e0 (ops imx8qm_ldb_ops)
[ 3.603605] imx6q-pcie 5f000000.pcie: iATU unroll: disabled
[ 3.612149] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /bus@56220000/dsi_host@56228000 to encoder DSI-149: -517
[ 3.617434] imx6q-pcie 5f000000.pcie: Detected iATU regions: 6 outbound, 6 inbound
[ 3.639547] max96789 5-0062: max96789_probe : max96789_probe start
[ 3.645770] max96789_probe : max96789_probe start
[ 3.674646] max96789 5-0062: max96789_probe : max96789_probe successfully
[ 3.683334] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.2 (ops dpu_bliteng_ops)
[ 3.691761] imx-drm display-subsystem: bound imx-drm-dpu-bliteng.5 (ops dpu_bliteng_ops)
[ 3.700383] imx-drm display-subsystem: bound imx-dpu-crtc.1 (ops dpu_crtc_ops)
[ 3.707911] imx-drm display-subsystem: bound imx-dpu-crtc.0 (ops dpu_crtc_ops)
[ 3.715620] imx-drm display-subsystem: bound imx-dpu-crtc.3 (ops dpu_crtc_ops)
[ 3.717492] imx6q-pcie 5f000000.pcie: Link up
[ 3.723306] imx-drm display-subsystem: bound imx-dpu-crtc.4 (ops dpu_crtc_ops)
[ 3.735227] imx-drm display-subsystem: bound bus@56240000:ldb@562410e0 (ops imx8qm_ldb_ops)
[ 3.744574] nwl-dsi 56228000.dsi_host: [drm:nwl_dsi_host_attach] lanes=4, format=0x0 flags=0x3
[ 3.753040] hub 3-1:1.0: USB hub found
[ 3.753423] imx-drm display-subsystem: bound 56228000.dsi_host (ops nwl_dsi_component_ops)
[ 3.757382] hub 3-1:1.0: 2 ports detected
[ 3.765767] [drm] Initialized imx-drm 1.0.0 20120507 for display-subsystem on minor 1
[ 3.780967] imx-drm display-subsystem: [drm] fb0: imx-drmdrmfb frame buffer device
[ 3.792732] debugfs: Directory 'lvds1' with parent 'pm_genpd' already present!
[ 3.800074] debugfs: Directory 'mipi1-i2c1' with parent 'pm_genpd' already present!
[ 3.808058] debugfs: Directory 'mipi1-i2c0' with parent 'pm_genpd' already present!
[ 3.815748] debugfs: Directory 'mipi1-pwm0' with parent 'pm_genpd' already present!
[ 3.823417] debugfs: Directory 'mipi1' with parent 'pm_genpd' already present!
[ 3.827227] imx6q-pcie 5f000000.pcie: Link up
[ 3.835028] imx6q-pcie 5f000000.pcie: Link up, Gen2
[ 3.836912] isi-m2m 58100000.isi:m2m_device: Register m2m success for ISI.0
[ 3.873117] ALSA device list:
[ 3.876094] No soundcards found.

 

root@cnh-pegasus:~# cat /proc/asound/cards
0 [add2010 ]: simple-card - add2010
                      add2010

root@cnh-pegasus:~# ls /dev/snd/
by-path controlC0 pcmC0D0p timer

 

Thanks

 

0 Kudos
Reply
1 Solution
1,971 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do not worry about it, I have test on our EVK BOARD, found the No sound cards found the same. Because not sound card are in using, I think it is the reason. The same with you, it is not the error or failed information, you can ignore it.

Rita_Wang_1-1715932383009.png

But in your log you can see it is already added success.

Rita_Wang_2-1715932600381.png

You can also see that all the sound card support in my side:

Rita_Wang_3-1715932631844.png

So it is OK in your side, no problem.

 

 

View solution in original post

0 Kudos
Reply
3 Replies
1,972 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Do not worry about it, I have test on our EVK BOARD, found the No sound cards found the same. Because not sound card are in using, I think it is the reason. The same with you, it is not the error or failed information, you can ignore it.

Rita_Wang_1-1715932383009.png

But in your log you can see it is already added success.

Rita_Wang_2-1715932600381.png

You can also see that all the sound card support in my side:

Rita_Wang_3-1715932631844.png

So it is OK in your side, no problem.

 

 

0 Kudos
Reply
1,999 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Are you using NXP reference board or the board you designed yourself?

0 Kudos
Reply
1,993 Views
simonlin
Contributor II

Hi @Rita_Wang 

We are using the board designed by ourselves

Do you have any suggestion?

Thanks

0 Kudos
Reply