Build Configuration:
BB_VERSION = "1.20.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-12.04"
TARGET_SYS = "arm-poky-linux-gnueabi"
MACHINE = "imx6dlsabresd"
DISTRO = "poky"
DISTRO_VERSION = "1.5.1"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa9"
TARGET_FPU = "vfp-neon"
meta
meta-yocto = "(nobranch):f1276b066223e7f501f7f711680215ff8edee252"
meta-oe = "(nobranch):40e0f371f3eb1628655c484feac0cebf810737b4"
meta-fsl-arm = "(nobranch):5fdb620c09df11e70434092f675c891e0ba84108"
meta-fsl-arm-extra = "(nobranch):251c07f9d868e0100ccf74fd1706269c8d6911fb"
meta-fsl-demos = "(nobranch):5a12677ad000a926d23c444266722a778ea228a7"
Hello,
first timer here. I tried to "bitbake fsl-image-gui".
I get these errors:
ERROR: Function failed: do_rootfs (log file is located at /home/chuck/work/fsl-community-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.15734)
ERROR: Logfile of failure stored in: /home/chuck/work/fsl-community-bsp/build/tmp/work/imx6dlsabresd-poky-linux-gnueabi/fsl-image-gui/1.0-r0/temp/log.do_rootfs.15734ERROR: Task 7 (/home/chuck/work/fsl-community-bsp/sources/meta-fsl-demos/recipes-fsl/images/fsl-image-gui.bb, do_rootfs) failed with exit code '1'
When I look in build/tmp/deploy/images/imx6dlsabresd/ there is no .sdcard image there.
Can anyone help?
Thanks,
Chuck
解決済! 解決策の投稿を見る。
Thank you for your time.
I'm sorry, I have little idea of what I'm doing.
I have a friend who tells me it may be something I put into the local.conf.
He told me to put back the original sample local.conf, do a -c clean and
see if it builds.
If it does, then it must be something I added to local.conf.
I'll contact you if this does not work.
Chuck Etzweiler | Integration Engineer
w. 814.235.1111 x394
e. chuck@videon-central.com
<http://www.videon-central.com>
<https://plus.google.com/u/0/104238493788225182046/posts>
<http://www.linkedin.com/company/videon-central>
<https://www.facebook.com/videon.central>
On Fri, Mar 28, 2014 at 2:09 PM, Daiane Angolini <
This error says me nothing.
Could you, please share more lines of the error?
Thank you for your time.
I'm sorry, I have little idea of what I'm doing.
I have a friend who tells me it may be something I put into the local.conf.
He told me to put back the original sample local.conf, do a -c clean and
see if it builds.
If it does, then it must be something I added to local.conf.
I'll contact you if this does not work.
Chuck Etzweiler | Integration Engineer
w. 814.235.1111 x394
e. chuck@videon-central.com
<http://www.videon-central.com>
<https://plus.google.com/u/0/104238493788225182046/posts>
<http://www.linkedin.com/company/videon-central>
<https://www.facebook.com/videon.central>
On Fri, Mar 28, 2014 at 2:09 PM, Daiane Angolini <