Hello,
Do you know any hardware and distro that support Netflix with the i.MX 5 or i.MX 6.
I own a Wandboard (i.mx 6) and a Sabrelite (i.mx 6) but the Netflix player does not seem to work out of the box on these devices.
Did anybody is using any I.MX hardware as a media center to watch Netflix video on a HD TV ?
Thanks
ssinfod
解決済! 解決策の投稿を見る。
Now the question is if the app takes advantage of HW Codec accelerators (VPU and IPU), does it?
Is there any error log when launching the player? Android?
I tried with Android on the Wandboard but I can't install the Netflix player from Google play.
https://play.google.com/store/apps/details?id=com.netflix.mediaclient
It seems the Wandboard is not an 'official' device in Google Play..
Where can I get the Netflix installer for the i.MX (or any ARM platform) ?
Thanks
ssinfod.
I got a reply from the wandboard forum..
Wandboard Discussion Forums • View topic - Netflix on Android ?
It seems Netflix is running in Android on the Wandboard.
I will try harder !!
Thanks,
ssinfod
Now the question is if the app takes advantage of HW Codec accelerators (VPU and IPU), does it?
OK, so I finally got it working on my wandboard dual.
I had to install google apps. (gapps)
Here is what I have done:
Inside a linux machine, I unzipped "gapps-jb-20130301-signed.zip", then I copied the uncompressed content to the "/media/system/" folder.
Commands:
cd ~/
mkdir gapps-jb
cd gapps-jb
unzip gapps-jb-20130301-signed.zip
sudo cp ~/gapps-jb/system/* /media/system/ -rf
sync
Then, I put the micro SD card back in the Wandboard. My wandboard has a WiFi connection.
After the reboot, the wandboard did some updates and then I had google "Play Store" in the Apps section.
I created a new google account in the Settings, Accounts section.
Then, I started the "Play Store" app and browse for the Netflix app (entertainment free app). Then I installed it with the Install button in the Google Play Store. After a few minutes (2-3 minutes), the Netflix apps was downloaded and it installed itself in the "Apps section".
I'm now able to see video from the Netflix apps.
However it is still running a bit slow... I see frames lagging...
I have a wandboard dual only running from SD card. (Lexar Class 10, 16GB)
Maybe the Wandboard quad has better performance... It would be great to try running Android from a SSD drive.
Thanks everybody for your support,
ssinfod