Need help on changing NAND type for i.MX287 WinCE 6.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help on changing NAND type for i.MX287 WinCE 6.0

498件の閲覧回数
MarcCoussement
Contributor I

Hi,

 

I need help on changing the nand type on the EVK for i.MX287 with WinCE

 

We use the 8GBIT MICRON MT29F8G08AAAWP on the EVK and this works fine. Now we need to use the 4GBIT MT29F4G08.

 

We have been reading the application notes for the i.MX35, 51, 25 but the FMD.CPP for the i.MX287 seems to use a different way of storing the parameters.

 

We can´t find any information for the i.MX287

 

All help appreciated.

 

Information on other freescale CPU´s:

 

Changing the i.MX35 NAND Flash Model for Windows Embedded CE 6.0 AN3976.pdf

Changing the i.MX51 NAND Flash Model for Windows Embedded CETM 6.0 AN3986.pdf

Changing the i.MX25 NAND Flash Model for Windows Embedded CE 6.0 AN4111.pdf

ラベル(1)
0 件の賞賛
0 返答(返信)