Need clarification about DRM drivers for i.mx6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need clarification about DRM drivers for i.mx6

2,993 次查看
kruglikov_dmt
Contributor III

Hi. I'm working with MCIMX6S5DVW10AC (IMX6 Solo). I noted that Linux kernel have two different DRM drivers:

* drivers/gpu/drm/vivante (also available in menuconfig as Vivante GCCore, selected for building and installation)

* drivers/gpu/drm/imx (not available in menuconfig)

What difference between these drivers?

Can you help me to check does DRM is enabled in my system (without X11)?

(I have troubles with application glmark2, it can't find any DRM devices in my system and fails with message "Failed to open DRM module 'imx-drm'").

Thanks!

标签 (4)
标记 (4)
0 项奖励
1 回复

2,350 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Eugene

what bsp used in the case, one can look at link below with nxp

linux documentation

i.MX Software | NXP 

Just for reference attached Linux Manual, one can check

Chapter 13 Graphics Processing Unit (GPU).

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励