Nand Image unpacking/extraction from IMX6 MCIMX6S5DVM10AC and S34ML04G100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nand Image unpacking/extraction from IMX6 MCIMX6S5DVM10AC and S34ML04G100

363 Views
IvanCherkayev
Contributor I

Hello everyone in this community!


i have a coffee machine running on MCIMX6S5DVM10AC processor with nand S34ML04G100.
OS: WINCE 7
open telnet and ftp ports
through the programmer, I took an image from nand: dump.bin 
(the image is working, I restored it to a new nand memory and the coffee machine started working.)
full log startup from console:  log startup.txt 
boot options:  Boot options.txt 

Can anyone share a tip for extracting a disk image? I want to know the telnet password. This password is also the FTP password.

what I need it for: I have a VNC server for this machine, it will help reduce the time for their maintenance. Price changes, configuration changes, and so on.

If more information is needed, I will provide it. I will be glad to any advice.

Thank you all!

Tags (2)
0 Kudos
1 Reply

329 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I see that you are using the WINCE 7, the wince  is unavailable from nxp, since it is out of date. Sorry about it, here you can try to search in the old thread to see if there is some useful link.

0 Kudos