NVCC power supply design on i.MX8M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVCC power supply design on i.MX8M

1,468 Views
chao
Contributor II

Hi everyone,

We are designing the circuit of i.MX8M Mini. If the peripherals in our design are all 3.3V interfaces, should the NVCC power pins (such as NVCC_JTAG/NVCC_NAND/NVCC_I2C/NVCC_GPIO1/NVCC_ECSPI/NVCC_SAI2) be connected to 3.3V?

Labels (1)
0 Kudos
Reply
2 Replies

1,456 Views
chao
Contributor II

Hi igor,

thank you reply again,

The following table lists the NVCC pins used in the reference design file. Some pins are connected to 1.8V, while others are connected to 3.3V. If our peripherals are all 3.3V interfaces. Do these pins whice connected to 1.8V need change to 3.3V?

 

Pin NumberPIN NAMEVoltage used in reference Design Files
L19NVCC_JTAG1.8V
U19NVCC_NAND3.3V
W18NVCC_SAI13.3V
V19NVCC_SAI21.8V
Y10NVCC_SAI33.3V
W17NVCC_SAI53.3V
W12NVCC_GPIO11.8V
J11NVCC_I2C1.8V
J12NVCC_UART1.8V
H10NVCC_ECSPI3.3V
W22NVCC_ENET1.8V
V20NVCC_SD11.8V
V22NVCC_SD21.8V
M19NVCC_CLK1.8V

 

0 Kudos
Reply

1,461 Views
igorpadykov
NXP Employee
NXP Employee

Hi liaochao

 

one needs to follow pad powering described in Table 85. i.MX 8M Dual / 8M QuadLite / 8M Quad 17 x 17 mm functional contact assignments, column "Power Group"

i.MX 8M Dual / 8M QuadLite / 8M Quad Applications Processors Data Sheet for Consumer Products

So first you should find which pad used in the case, then using that table find power "NVCC***" for it.

 

Best regards
igor

0 Kudos
Reply