Hi,
I just started exploring with i.MX8MQEVK.
I flshed the pre-build image “LF_v5.10_2.0.0_images_IMX8MQEVK.zip” which is available at NXP site.
Then i connect IMX-MIPI-HDMI exactly in the same way as mentioned in the document link “Quick Start Guide for IMX-MIPI-HDMI for i.MX 8M Evaluation Kit” and followed the same step.
I also connected a screen through HDMI (one end at the MIPI-HDMI and the other end at the monitor screen) and expected to see the image on HDMI monitor after boot completes.
Also, while booting the board i am getting the below lines
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
Not sure if this is causing the problem.
Can you please help me in this?
Thanks,
Priyanshu
I found the reason, you should change the fdt_file to imx8mq-evk-dcss-adv7535.dtb right, in the latest bsp, use fdtfile to replace fdt_file, so try to "setenv fdtfile imx8mq-evk-dcss-adv7535.dtb" then "saveenv"