NAND, flashing bootloader(u-boot.bin) with kobs-ng tool error.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND, flashing bootloader(u-boot.bin) with kobs-ng tool error.

4,686件の閲覧回数
YamilGarcia
Contributor III

I'm working with a custom board based in  sabrelite platform, basically it is a sabrelite with NAND support.

When I try to flash the bootloader(u-boot.bin) with kobs-ng tool, it always prompt me an error.

The kernel GPMI driver find the NAND device successfully and partitions are created correctly as shown below:

Kernel GPMI driver output:

ONFI flash detected

ONFI param page 0 valid

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron MT29F8G08ADADAH4)

gpmi-nand imx6q-gpmi-nand.0: enable asynchronous EDO mode 5

3 cmdlinepart partitions found on MTD device gpmi-nand

Creating 3 MTD partitions on "gpmi-nand":

0x000000000000-0x000000100000 : "boot"

0x000000100000-0x000000500000 : "kernel"

0x000000500000-0x000040000000 : "rootfs"

GPMI NAND driver registered. (IMX)

mtd partitions:

root@freescale /$ cat /proc/mtd

dev:    size   erasesize  name

mtd0: 00100000 00020000 "boot"

mtd1: 00400000 00020000 "kernel"

mtd2: 3fb00000 00020000 "rootfs"

kobs-ng output:

root@freescale /$ kobs-ng init -v u-boot.bin

MTD CONFIG:

  chip_0_device_path = "/dev/mtd0"

  chip_1_device_path = "(null)"

  search_exponent = 2

  data_setup_time = 80

  data_hold_time = 60

  address_setup_time = 25

  data_sample_time = 6

  row_address_size = 3

  column_address_size = 2

  read_command_code1 = 0

  read_command_code2 = 48

  boot_stream_major_version = 1

  boot_stream_minor_version = 0

  boot_stream_sub_version = 0

  ncb_version = 3

  boot_stream_1_address = 0

  boot_stream_2_address = 0

u-boot.bin: verifying using key '00000000000000000000000000000000'

u-boot.bin: is a valid bootstream for key '00000000000000000000000000000000'

mtd: opening: "/dev/mtd0"

NFC geometry :

        ECC Strength       : 8

        Page Size in Bytes : 2112

        Metadata size      : 10

        ECC Chunk Size in byte : 512

        ECC Chunk count        : 4

        Block Mark Byte Offset : 1999

        Block Mark Bit Offset  : 0

====================================================

mtd: opened '/dev/mtd0' - '(null)'

mtd: bootstream too large

mtd_init failed!

Can someone give a hint on this, please?

Thanks in advance.

ラベル(5)
0 件の賞賛
返信
4 返答(返信)

1,657件の閲覧回数
YixingKong
Senior Contributor IV

Yamil, please respond Grace's question. Yur discussion may be closed if no repy in next two days.

Thanks,

Yixing

0 件の賞賛
返信

1,657件の閲覧回数
Raana
Contributor III

Hi Yixing,

I am also facing the same issue but some what different.

Mine is,

/mnt/mmcblk1p1/u-boot.bin: verifying using key '00000000000000000000000000000000'

/mnt/mmcblk1p1/u-boot.bin: is a valid bootstream for key '00000000000000000000000000000000'

mtd: opening: "/dev/mtd0"

mtd: device /dev/mtd0 can't ioctl MEMGETOOBSEL: -1

Unable to open mtd device(s)

But at the same time I am able to save the environment and boot the uImage from NAND.

Herewith, I attached the full log file of this issue.

0 件の賞賛
返信

1,657件の閲覧回数
GraceH
Senior Contributor II

Hi Yamil Garcia,

What is the size of your u-boot.bin?  mtd0 size is small and your u-boot.bin can't fit in.

The boot area will contain both search areas and two copies of the boot stream.

Grace

1,657件の閲覧回数
YamilGarcia
Contributor III

Yes, you were right, the problem was the size of partition.

I already fixed it and it is working fine. I was able to flash u-boot in NAND.

Thanks to all in the community for their support.

0 件の賞賛
返信