I have ported the mt9v022 driver from soc camera model to platform camera model as used in ov5642 driver present in the imx kernel (3.14.54v). And I added the device tree node for the image sensor. The driver is getting loaded and when I use v4l2-clt to capture image it shows time out error.
Board details: imx6qsabresd platform
capture command:
$ v4l2-ctl --stream-mmap=3 --stream-count=1 --stream-to=gt.jpeg
Error details:
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
debug messages:
In MVC: mxc_v4l_open
device name is Mxc Camera
In g_ifparm function
In ioctl_g_fmt_cap function
End of mxc_v4l_open: v2f pix widthxheight 288 x 352
End of mxc_v4l_open: crop_bounds widthxheight 640 x 480
End of mxc_v4l_open: crop_defrect widthxheight 640 x 480
End of mxc_v4l_open: crop_current widthxheight 640 x 480
On Open: Input to ipu size is 640 x 480
ipu csi init interface
In s_power function
In standby function
In ioctl_init function
In dev_init function
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 80685600
case VIDIOC_QUERYCAP
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0e85667
case default or not supported
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445624
case VIDIOC_REQBUFS
In MVC:mxc_streamoff
MVC: In mxc_free_frame_buf
In MVC:mxc_allocate_frame_buf - size=152064
cma: dma_alloc_from_contiguous(cma 80e0719c, count 38, align 6)
cma: dma_alloc_from_contiguous(): returned abcd9000
cma: dma_alloc_from_contiguous(cma 80e0719c, count 38, align 6)
cma: dma_alloc_from_contiguous(): returned abcd9800
cma: dma_alloc_from_contiguous(cma 80e0719c, count 38, align 6)
cma: dma_alloc_from_contiguous(): returned abcda000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x3c100, start=0x76a53000, end=0x76a79000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x3c140, start=0x76a2d000, end=0x76a53000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445609
case VIDIOC_QUERYBUF
In MVC:mxc_v4l2_buffer_status
In MVC:mxc_mmap
pgoff=0x3c180, start=0x76a07000, end=0x76a2d000
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c044560f
case VIDIOC_QBUF
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 40045612
case VIDIOC_STREAMON
In MVC:mxc_streamon
camera enable
In irq request
YUV420
IN IPU Enable CSI and enabling csi: 0
CSI 0 Enabled<6>Enabled CSI
In MVC:mxc_poll
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl c0445611
case VIDIOC_DQBUF
In MVC:mxc_v4l_dqueue
galcore 130000.gpu: pm_genpd_runtime_resume()
galcore 130000.gpu: pm_genpd_runtime_suspend()
ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0
In MVC:mxc_v4l_ioctl
In MVC: mxc_v4l_do_ioctl 40045613
case VIDIOC_STREAMOFF
In MVC:mxc_streamoff
IN IPU Disable CSI and disabling csi: 0
In irq requestCSI 0 Disabled
cma: dma_release_from_contiguous(page abcda800)
In MVC:mxc_free_frames
In MVC:mxc_v4l_close
In MVC:mxc_streamoff
In s_power function
In standby function
mxc_v4l_close: release resource
MVC: In mxc_free_frame_buf
cma: dma_release_from_contiguous(page abcd9000)
cma: dma_release_from_contiguous(page abcd9800)
cma: dma_release_from_contiguous(page abcda000)
In MVC:mxc_free_frames
Any help would be great.
Hi Guna,
I am porting mt9v034 on imx6q, toradex board. there's a lot stuff needed to be done , as the project is very urgent , could you please post or send me your mt9v022 porting code so I can use it as a reference ? I am working on monochrome/color CMOS sensor driver porting and algorithm development , maybe we could discuss it and help each other afterwards.
My email address is guanlinbo@supcon.com. Thanks a lot!
Hi Gunasekaran
I think you can look at implementation of mt9v022 driver in phytec
releases (though for older kernels), as module VM-010 (Mt9v022) in
ftp://ftp.phytec.com/products/PFL-A-02_phyFLEX-iMX6/Linux/PD13.2.2/
then port it to device tree kernel using attached Porting Guide
Chapter 7 Supporting the i.MX 6Dual/6Quad/6Solo/6DualLite Camera Sensor with CSI
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
Thanks for the prompt reply.
I have ported the mt9v022 driver code (present under soc_camera) from Phytec BSP only. I have converted the platform data of mt9v022 to "OF" node data in the device tree. I am able to load the driver and initialize the IPU unit and when I give stream, I can trace the VIDIOC_STREAMON IOCTL being called. But I am getting error in TIMEOUT in waiting for the frame buffer.
Thanks,
Guna
Hi Igor,
What is the imx_test? Is it some test code available in fsl-community-bsp?
And one more thing. What about the CSI0_DATA_EN pin? Whether it should be enabled or disabled? Currently, in sabresd, that pin is connected to PCI_WAKE.
Thanks,
Guna
Hi Guna
http://repository.timesys.com/buildsources/i/imx-test/imx-test-3.14.28-1.0.0/
Best regards
igor
Hi Igor,
I have added the debug messages in enable_irq, request_irq, disable_irq and clear_irq function present in drivers/mxc/ipu3/ipu_common.c. I have attached the debug messages.
Could you direct me on how to handle this?
Debug messages:
NR_IRQS:16 nr_irqs:16 16
In irq request and Irq no=23
In err disable and irq no=23
In irq request and Irq no=87
In err disable and irq no=87
In irq request and Irq no=51
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In irq enable and enabling irq = 23
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq request and Irq no=451
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq request and Irq no=27
In err disable and irq no=27
In irq request and Irq no=91
In err disable and irq no=91
In irq request and Irq no=31
In clear irq and irq no=1
In err disable and irq no=27
In clear irq and irq no=1
In err disable and irq no=91
In irq request and Irq no=23
In err disable and irq no=23
In irq request and Irq no=87
In err disable and irq no=87
In irq request and Irq no=51
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq Handler and handling irq = 40
In irq request and Irq no=27
In err disable and irq no=27
In irq request and Irq no=91
In err disable and irq no=91
In irq request and Irq no=31
In clear irq and irq no=1
In err disable and irq no=27
In clear irq and irq no=1
In err disable and irq no=91
In irq request and Irq no=28
In err disable and irq no=28
In irq request and Irq no=92
In err disable and irq no=92
In clear irq and irq no=1
In err disable and irq no=28
In clear irq and irq no=1
In err disable and irq no=92
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq Handler and handling irq = 40
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq request and Irq no=451
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq Handler and handling irq = 40
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq request and Irq no=451
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq request and Irq no=451
In irq Handler and handling irq = 40
In irq Handler and handling irq = 40
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq request and Irq no=451
In irq Handler and handling irq = 40
In clear irq and irq no=1
In irq enable and enabling irq = 23
In irq request and Irq no=451
In irq Handler and handling irq = 40
In irq Handler and handling irq = 40
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In irq request and Irq no=451
In irq Handler and handling irq = 40
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
In clear irq and irq no=1
In err disable and irq no=23
In clear irq and irq no=1
In err disable and irq no=87
Thanks,
Gunasekaran S
Hi Guna
mt9v022 driver is not supported in official nxp bsp releases, for porting drivers
one can apply to NXP Professional Services:
http://www.nxp.com/pages/freescale-professional-services:PROFESSIONAL-SERVICES
Best regards
igor
Hi Igor,
I feel the problem is with the IPU interrupt registration and nothing to do with MT9v022 driver per say. Could you direct me on how to handle the interrupt request?
And I am getting this error even without MT9V022 driver i.e with only ov5642_camera.
Thanks
Guna