Mirasol Display Module compatible with i.MX6SL or not?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mirasol Display Module compatible with i.MX6SL or not?

742件の閲覧回数
baydoanvan
Contributor I

Dear community,


Currently, We start designing SmartWatch use Freescale i.MX6SL solution: http://www.freescale.com/webapp/sps/site/application.jsp?code=APLSMARTWATCH

We are using Mirasol Display Module, information about feartures and timing charateristics of it assigned in the attachment.

This module used MIPI DBI Type-B Parallel Interface. We see that the Timing diagram of Mirasol Module is compatible with timing diagram of eLCDIF mode of i.MX6SL. So that I think we can use the eLCDIF mode to turn on the Mirasol module.

Am I right?

Please tell me that it can communicate with i.MX6SL or not?


Best regards.

Bay

ラベル(1)
0 件の賞賛
返信
1 返信

568件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Yes, from attached diagrams this LCD can be used with eLCDIF i.MX6SL.

You also should check LCD IO levels for compatibility with i.MX6SL.

0 件の賞賛
返信