Mirasol Display Module compatible with i.MX6SL or not?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mirasol Display Module compatible with i.MX6SL or not?

682 Views
baydoanvan
Contributor I

Dear community,


Currently, We start designing SmartWatch use Freescale i.MX6SL solution: http://www.freescale.com/webapp/sps/site/application.jsp?code=APLSMARTWATCH

We are using Mirasol Display Module, information about feartures and timing charateristics of it assigned in the attachment.

This module used MIPI DBI Type-B Parallel Interface. We see that the Timing diagram of Mirasol Module is compatible with timing diagram of eLCDIF mode of i.MX6SL. So that I think we can use the eLCDIF mode to turn on the Mirasol module.

Am I right?

Please tell me that it can communicate with i.MX6SL or not?


Best regards.

Bay

Labels (1)
0 Kudos
Reply
1 Reply

508 Views
igorpadykov
NXP Employee
NXP Employee

Yes, from attached diagrams this LCD can be used with eLCDIF i.MX6SL.

You also should check LCD IO levels for compatibility with i.MX6SL.

0 Kudos
Reply