Minimum size of uimage on RAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Minimum size of uimage on RAM

1,044件の閲覧回数
arifsh10
Contributor I

Hi ,

      I am planning to use imx6ull. I want to know how much minimum RAM is required for bare minimum linux kernel for  imx6ULL system. Thanks .

0 件の賞賛
返信
1 返信

893件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Arif Shaikh,

There is not a definite answer to this, but this is a great answer given on another thread that has a very good approach.

"How much RAM is used by the kernel is a fuzzy subject as it is composed of various pieces. This is a more general Linux question not tied specifically to the NXP BSP. Having more RAM available allows Linux to cache better, avoiding slow, power-consuming flash reads and writes, etc. A dump of my /proc/meminfo (mem=256M) follows which has udevd, udhcpc, BusyBox syslogd & klogd and one getty running — minimal indeed.

 

The NXP i.MX 6UL EVK board has 512 MiB of DRAM. Measurements here translate 1:1 to the 6ULL. If I tell the kernel to use only 128 MiB on the kernel command line (mem=128M) the system boots to the login prompt, but one or more boot processes fail to allocate memory. I'd stick to at least 256 MiB for a small application."

 

root@imx6ulevk:~# cat /proc/meminfo
MemTotal:         247464 kB
MemFree:          195596 kB
MemAvailable:     197240 kB
Buffers:            1440 kB
Cached:             4784 kB
SwapCached:            0 kB
Active:             5232 kB
Inactive:           1920 kB
Active(anon):        980 kB
Inactive(anon):      148 kB
Active(file):       4252 kB
Inactive(file):     1772 kB
Unevictable:           0 kB
Mlocked:               0 kB
HighTotal:             0 kB
HighFree:              0 kB
LowTotal:         247464 kB
LowFree:          195596 kB
SwapTotal:             0 kB
SwapFree:              0 kB
Dirty:                 0 kB
Writeback:             0 kB
AnonPages:           948 kB
Mapped:             3152 kB
Shmem:               200 kB
Slab:               7076 kB
SReclaimable:       2196 kB
SUnreclaim:         4880 kB
KernelStack:         400 kB
PageTables:          168 kB
NFS_Unstable:          0 kB
Bounce:                0 kB
WritebackTmp:          0 kB
CommitLimit:      123732 kB
Committed_AS:       3924 kB
VmallocTotal:    1810432 kB
VmallocUsed:       37908 kB
VmallocChunk:    1596104 kB
CmaTotal:              0 kB
CmaFree:               0 kB

I hope this helps!

Regards,

0 件の賞賛
返信