Command:
gst-launch-1.0 playbin uri=rtsp://192.168.1.88:556/vga
The memory of gst-launch-1.0 will increase more than 30M every hour, then the video stop, but audio soud ok。
Delete the libgstvpu.so , use the same commad. memory will not increase, but play the high resolution (1920x1080) not smooth.
Anybody has faced the same problem and resolved? Please help
I do more test.
Compare playing local video file and RTSP:
1) play 1920x1080 ((MPEG4\AVC_H_L3)local files, that seems not has memory leak. (log file : gplay-test-AVC_H_L3_Schindlers.log、gplay-test-MPEG4_Schindlers.log)
2) play 1920x1080 (AVC_H) RTSP, memory increase about 16M. (log file: gplay-test-AVC_H_RTSP.log)
Compare playing RTSP(960x540 AVC_H) with vpudec and avdec_h264 lib:
a) use vpudec , memory increase about 10M in 20 mins.( log file: gplay-test-AVC_H_RTSP_with_VPU.log)
b) use avdec_h264(delete /usr/lib/gstreamer-1.0/libgstvpu.so) , memory not increase. (log file: gplay-test-AVC_H_RTSP_with_avdec_h264.log)
CPU: IMX6DL
Kernel: 4.1.15
BSP: 2.0.1 GA
vpudec: imx-gst1.0-plugin-4.1.4
avdec_h264:gst-libav-1.8.1
Can you show us some h264parse and vpu log after applying the "Set-min_frame_size-of-h264parse-to-10.patch"?
Just input debug command line "export GST_DEBUG=h264parse:6,vpu_dec_object:6" on board first, then start to play the rtsp stream.
Ten minites' log is enough and we will check whether the patch works in your side.
With play_log_with_debug.rar from you after applying the patch, h264parse receive the same 9bytes frame(type=SEI, size=5) for every 15 frames. It is now pushed downstream with the next IDR frame as what patch expected. Then vpu decode each frame it received and list length of frames won't increase.
"[05-28-15:00:25.072]0:01:37.288456012 7033 0x790120 DEBUG h264parse gsth264parse.c:717:gst_h264_parse_process_nal:<h264parse0> processing nal of type 6 SEI, size 5"
With RTSP_memory_2019-05-27.rar from you, memory usage of gplay-1.0 is almost stable from 19:00-22:00 at 427M, but increase at 17:00-19:00 from 378M to 427M.
In our side, with the patch, vpu can decode each frame it received and send out the same as you. The memory usage of gst-launch-1.0/gplay-1.0 is 21256 after 1 minute's play. Attached memory-record.log
HI, Qiang:
But why my video will still pause for a long time.
What is the resolution of rtsp://192.168.1.98:8554/vga now? If the resolution is litte , the memory will not increase. My hdmi encoder output resolution is 1920x1080.
From our debug, the memory leak issue is same for 720P and 1080P. Your log is not aligned with our side, it increased at first two houres, then keep there for followed three houres.
And our log always show the same memory size. Maybe you can also try with 720P.
The memory will not increase when up to 400m+, but the video will pause about 3mins, then continue to play.
I found the memory increase immediately when play with http scream if show this log "gst_base_sink_is_too_late:<overlaysink0> warning: A lot of buffers are being dropped."
Was this problem cause when vpudec fail not but free the memory about frame?
I'm not familiar with vpudec follow, please give me some advice.
Wait for your reply.
thanks for reply, but this problem is still there.
b36401 please give more help.
The problem is urgent, because this product has been mass-produced for more than 1 years.
CPU: IMX6DL
Kernel: 4.1.15
BSP: 2.0.1 GA
GST: imx-gst1.0-plugin-4.1.4