Mask Set Errata for Mask 3N09P ID No. e9165

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mask Set Errata for Mask 3N09P ID No. e9165

Jump to solution
633 Views
goto11
Contributor III

Hello,Community

There is a description of “eCSPI: TXFIFO empty flag glitch can cause the current FIFO transfer to be sent twice”.
Is this description not applicable to Quad Serial Peripheral Interface (QuadSPI)?

best regards

Goto

Labels (1)
0 Kudos
Reply
1 Solution
558 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

right, it is not applicable to QuadSPI module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
559 Views
igorpadykov
NXP Employee
NXP Employee

Hi Goto

right, it is not applicable to QuadSPI module.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply