i have marvell 8787 based wifi module.
http://www.t-yuden.com/wireless/WYSBMVGXB.pdf
I want to interface it with imx6qsabresd board running yocto 3.14.28.1.0.1 based linux.
when i connect it to SD2 slot following message appear in terminal.
mmc1: new high speed SDIO card at address 0001
i have driver .bin file and source code with me.
So how to start?
Hi,
I think you need to install the driver and update the firmware like in the below links:
How to setup Marvell 88w8686 SDIO wifi - IGEP Community Wiki
Linux Kernel Driver DataBase: CONFIG_MWIFIEX_SDIO: Marvell WiFi-Ex Driver for SD8787/SD8797
Best Regards,
Alejandro
thanks for the reply.
in the first link they said to add libertas module by following command
modprobe libertas_sdio
But as you can see in the above attached image of Kconfig there is no libertas available for sd8787.
So how to get this?
And i have source code of the wi-fi module but i unable to cross compile it.
So can you tell me how to cross compile it with my board's linux version 3.14.28?
i have find suppoert for marvel 8787 in kernel config
and enable Marwell wifi-ex driver and marvell 8xxx WLAN deiver.
and build kernel image.
And also i added "sd8787_uapsta.bin" in lib/firmware/mrvl in folder.
And after that when i insert the module i got following message
mmc1: new high speed SDIO card at address 0001
mwifiex_sdio mmc1:0001:1: WLAN FW is active
ieee80211 phy0: ignoring F/W country code US
mwifiex_sdio mmc1:0001:1: driver_version = mwifiex 1.0 (14.66.9.p80)
and iwconfig gives me following output
sit0 no wireless extensions.
lo no wireless extensions.
mlan0 no wireless extensions.
eth0 no wireless extensions.
and ifconfig not showing me any wifi device.
So whats the problem?
and how to enable module?
And can mlan.ko & sd8787.ko can available for Linux imx6qsabresd 3.14.28-1.0.0_ga+g91cf351? So i can add this instead of mwifiex_sdio.ko?