Macraigor jtag

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Macraigor jtag

1,236 次查看
christophe
Contributor V

Hi,

I've tried a usb2demon device on a QSB board and it doesn't work at all.

I've seen that QSB board have a 1,8V ref tension on its jtag connector (pin 1) and usb2demon is waiting for a tension going from 2.2 to 5 V. Do you think it could be the problem.

What's the type of Macraigor's device used with imx53qsb ?

Thanks.

标签 (1)
0 项奖励
回复
4 回复数

1,047 次查看
JamesMacGregor
Contributor I

Macraigor Systems will have a demo of our Usb2Demon and Eclipse Indigo/gnutools running on the iMX53 Quick Start board at ESC San Jose this week (tuesday - thursday).

Some of our old ARM20 Usb2Demons were built with drivers that only supported 2.5V and higher. If you need one that supports the lower voltage value. Email me at jamesm@macraigor.com and we will exchange your unit for the newer lower voltage version.

0 项奖励
回复

1,047 次查看
FlorentAuger
Contributor V

Hello,

I suggest you to contact the JTAG tool manufacturer. Macraigor is used to work with Freescale product.

In the meantime, I would replace R157 by a 0ohm instead of the default 100ohm which is actually not necessary. That avoids an additional slight voltage drop for the reference.

0 项奖励
回复

1,047 次查看
IvicaEftimovski
Contributor III

I used the plain LTIB provided gdb with Segger as server. I haven't done any Android development (yet), so I cannot help you much there.

0 项奖励
回复

1,047 次查看
IvicaEftimovski
Contributor III

I actually don't have a very good experience with Macraigor JTAG/BDMs under Linux, but other people may differ. For the iMX535QSB, I started using SEGGER J-link for ARM www.segger.com/jlink.html and it works great under both Linux and Windows. It did not support iMX535 out of the box, but it does update its firmware when connected. After the firmware update it worked just fine.

0 项奖励
回复